ZHCSK74A August 2019 – April 2020 DRV425-Q1
PRODUCTION DATA.
Decouple both VDD pins of the DRV425-Q1 with 1-µF, X7R-type ceramic capacitors to the adjacent GND pin, as illustrated in Figure 76. For best performance, place both decoupling capacitors as as possible close to the related power-supply pins. Connect these capacitors to the power-supply source in a way that allows the current to flow through the pads of the decoupling capacitors.