ZHCSCJ7E July 2013 – June 2014 CC3200
PRODUCTION DATA.
Figure 3-1 shows pin assignments for the 64-pin QFN package.
Figure 3-1 QFN 64-Pin Assignments
The device makes extensive use of pin multiplexing to accommodate the large number of peripheral functions in the smallest possible package. To achieve this configuration, pin multiplexing is controlled using a combination of hardware configuration (at device reset) and register control.
NOTE
TI highly recommends using the CC3200 pin multiplexing utility to obtain the desired pinout.
The board and software designers are responsible for the proper pin multiplexing configuration. Hardware does not ensure that the proper pin multiplexing options are selected for the peripherals or interface mode used.
Table 3-1 describes the general pin attributes and presents an overview of pin multiplexing. All pin multiplexing options are configurable using the pin mux registers.
The following special considerations apply:
NOTE
If an external device drives a positive voltage to the signal pads and the CC3200 device is not powered, DC current is drawn from the other device. If the drive strength of the external device is adequate, an unintentional wakeup and boot of the CC3200 device can occur. To prevent current draw, TI recommends any one of the following:
| General Pin Attributes | Function | Pad States | |||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| Pkg Pin | Pin Alias | Use | Select as Wakeup Source | Config Addl Analog Mux | Muxed with JTAG | Dig. Pin Mux Config Reg | Dig. Pin Mux Config Mode Value | Signal Name | Signal Description | Signal Direction | LPDS(1) | Hib(2) | nRESET = 0 |
| 1 | GPIO10 | I/O | No | No | No | GPIO_PAD_CONFIG_10 (0x4402 E0C8) |
0 | GPIO10 | General-Purpose I/O | I/O | Hi-Z | Hi-Z | Hi-Z |
| 1 | I2C_SCL | I2C Clock | O (Open Drain) |
Hi-Z | |||||||||
| 3 | GT_PWM06 | Pulse-Width Modulated O/P | O | Hi-Z | |||||||||
| 7 | UART1_TX | UART TX Data | O | 1 | |||||||||
| 6 | SDCARD_CLK | SD Card Clock | O | 0 | |||||||||
| 12 | GT_CCP01 | Timer Capture Port | I | Hi-Z | |||||||||
| 2 | GPIO11 | I/O | Yes | No | No | GPIO_PAD_CONFIG_11 (0x4402 E0CC) |
0 | GPIO11 | General-Purpose I/O | I/O | Hi-Z | Hi-Z | Hi-Z |
| 1 | I2C_SDA | I2C Data | I/O (Open Drain) |
Hi-Z | |||||||||
| 3 | GT_PWM07 | Pulse-Width Modulated O/P | O | Hi-Z | |||||||||
| 4 | pXCLK (XVCLK) | Free Clock To Parallel Camera | O | 0 | |||||||||
| 6 | SDCARD_CMD | SD Card Command Line | I/O | Hi-Z | |||||||||
| 7 | UART1_RX | UART RX Data | I | Hi-Z | |||||||||
| 12 | GT_CCP02 | Timer Capture Port | I | Hi-Z | |||||||||
| 13 | McAFSX | I2S Audio Port Frame Sync | O | Hi-Z | |||||||||
| 3 | GPIO12 | I/O | No | No | No | GPIO_PAD_CONFIG_12 (0x4402 E0D0) |
0 | GPIO12 | General Purpose I/O | I/O | Hi-Z | Hi-Z | Hi-Z |
| 3 | McACLK | I2S Audio Port Clock O | O | Hi-Z | |||||||||
| 4 | pVS (VSYNC) | Parallel Camera Vertical Sync | I | Hi-Z | |||||||||
| 5 | I2C_SCL | I2C Clock | I/O (Open Drain) |
Hi-Z | |||||||||
| 7 | UART0_TX | UART0 TX Data | O | 1 | |||||||||
| 12 | GT_CCP03 | Timer Capture Port | I | Hi-Z | |||||||||
| 4 | GPIO13 | I/O | Yes | No | No | GPIO_PAD_CONFIG_13 (0x4402 E0D4) |
0 | GPIO13 | General-Purpose I/O | I/O | Hi-Z | Hi-Z | Hi-Z |
| 5 | I2C_SDA | I2C Data | I/O (Open Drain) |
||||||||||
| 4 | pHS (HSYNC) | Parallel Camera Horizontal Sync | I | ||||||||||
| 7 | UART0_RX | UART0 RX Data | I | ||||||||||
| 12 | GT_CCP04 | Timer Capture Port | I | ||||||||||
| 5 | GPIO14 | I/O | No | No | GPIO_PAD_CONFIG_14 (0x4402 E0D8) |
0 | GPIO14 | General-Purpose I/O | I/O | Hi-Z | Hi-Z | Hi-Z | |
| 5 | I2C_SCL | I2C Clock | I/O (Open Drain) |
||||||||||
| 7 | GSPI_CLK | General SPI Clock | I/O | ||||||||||
| 4 | pDATA8 (CAM_D4) | Parallel Camera Data Bit 4 | I | ||||||||||
| 12 | GT_CCP05 | Timer Capture Port | I | ||||||||||
| 6 | GPIO15 | I/O | No | No | GPIO_PAD_CONFIG_15 (0x4402 E0DC) |
0 | GPIO15 | General-Purpose I/O | I/O | Hi-Z | Hi-Z | Hi-Z | |
| 5 | I2C_SDA | I2C Data | I/O (Open Drain) |
||||||||||
| 7 | GSPI_MISO | General SPI MISO | I/O | ||||||||||
| 4 | pDATA9 (CAM_D5) | Parallel Camera Data Bit 5 | I | ||||||||||
| 13 | GT_CCP06 | Timer Capture Port | I | ||||||||||
| 7 | GPIO16 | I/O | No | No | GPIO_PAD_CONFIG_16 (0x4402 E0E0) |
0 | GPIO16 | General-Purpose I/O | I/O | Hi-Z | Hi-Z | Hi-Z | |
| Hi-Z | |||||||||||||
| Hi-Z | |||||||||||||
| 7 | GSPI_MOSI | General SPI MOSI | I/O | Hi-Z | |||||||||
| 4 | pDATA10 (CAM_D6) | Parallel Camera Data Bit 6 | I | Hi-Z | |||||||||
| 5 | UART1_TX | UART1 TX Data | O | 1 | |||||||||
| 13 | GT_CCP07 | Timer Capture Port | I | Hi-Z | |||||||||
| 8 | GPIO17 | I/O | Wake-Up Source | No | No | GPIO_PAD_CONFIG_17 (0x4402 E0E4) |
0 | GPIO17 | General-Purpose I/O | I/O | Hi-Z | Hi-Z | Hi-Z |
| 5 | UART1_RX | UART1 RX Data | I | ||||||||||
| 7 | GSPI_CS | General SPI Chip Select | I/O | ||||||||||
| 4 | pDATA11 (CAM_D7) | Parallel Camera Data Bit 7 | I | ||||||||||
| 9 | VDD_DIG1 | Int pwr | N/A | N/A | N/A | N/A | N/A | VDD_DIG1 | Internal Digital Core Voltage | ||||
| 10 | VIN_IO1 | Sup. input | N/A | N/A | N/A | N/A | N/A | VIN_IO1 | Chip Supply Voltage (VBAT) | ||||
| 11 | FLASH_SPI_ CLK |
O | N/A | N/A | N/A | N/A | N/A | FLASH_SPI_ CLK |
Clock To SPI Serial Flash (Fixed Default) | O | Hi-Z(3) | Hi-Z | Hi-Z |
| 12 | FLASH_SPI_DOUT | O | N/A | N/A | N/A | N/A | N/A | FLASH_SPI_ DOUT |
Data To SPI Serial Flash (Fixed Default) | O | Hi-Z(3) | Hi-Z | Hi-Z |
| 13 | FLASH_SPI_ DIN |
I | N/A | N/A | N/A | N/A | N/A | FLASH_SPI_ DIN |
Data From SPI Serial Flash (Fixed Default) | I | |||
| 14 | FLASH_SPI_ CS |
O | N/A | N/A | N/A | N/A | N/A | FLASH_SPI_ CS |
Chip Select To SPI Serial Flash (Fixed Default) | O | 1 | Hi-Z | Hi-Z |
| 15 | GPIO22 | I/O | No | No | No | GPIO_PAD_CONFIG_22 (0x4402 E0F8) |
0 | GPIO22 | General-Purpose I/O | I/O | Hi-Z | Hi-Z | Hi-Z |
| 7 | McAFSX | I2S Audio Port Frame Sync | O | Hi-Z | |||||||||
| 5 | GT_CCP04 | Timer Capture Port | I | ||||||||||
| 16 | TDI | I/O | No | No | MUXed with JTAG TDI | GPIO_PAD_CONFIG_23 (0x4402 E0FC) |
1 | TDI | JTAG TDI. Reset Default Pinout. | I | Hi-Z | Hi-Z | Hi-Z |
| 0 | GPIO23 | General-Purpose I/O | I/O | ||||||||||
| 2 | UART1_TX | UART1 TX Data | O | 1 | |||||||||
| 9 | I2C_SCL | I2C Clock | I/O (Open Drain) |
Hi-Z | |||||||||
| 17 | TDO | I/O | Wake-Up Source | No | MUXed with JTAG TDO | GPIO_PAD_CONFIG_ 24 (0x4402 E100) |
1 | TDO | JTAG TDO. Reset Default Pinout. | O | Hi-Z | Hi-Z | Hi-Z |
| 0 | GPIO24 | General-Purpose I/O | I/O | ||||||||||
| 5 | PWM0 | Pulse Width Modulated O/P | O | ||||||||||
| 2 | UART1_RX | UART1 RX Data | I | ||||||||||
| 9 | I2C_SDA | I2C Data | I/O (Open Drain) |
||||||||||
| 4 | GT_CCP06 | Timer Capture Port | I | ||||||||||
| 6 | McAFSX | I2S Audio Port Frame Sync | O | ||||||||||
| 18 | GPIO28 | I/O | No | GPIO_PAD_CONFIG_ 28 (0x4402 E110) |
0 | GPIO28 | General-Purpose I/O | I/O | Hi-Z | Hi-Z | Hi-Z | ||
| 19 | TCK | I/O | No | No | MUXed with JTAG/SWD-TCK | 1 | TCK | JTAG/SWD TCK Reset Default Pinout | I | Hi-Z | Hi-Z | Hi-Z | |
| 8 | GT_PWM03 | Pulse Width Modulated O/P | O | ||||||||||
| 20 | TMS | I/O | No | No | MUXed with JTAG/SWD-TMSC | GPIO_PAD_CONFIG_ 29 (0x4402 E114) |
1 | TMS | JATG/SWD TMS Reset Default Pinout | I/O | Hi-Z | Hi-Z | Hi-Z |
| 0 | GPIO29 | General-Purpose I/O | |||||||||||
| 21(4)(5) | SOP2 | O Only | No | No | No | GPIO_PAD_CONFIG_ 25 (0x4402 E104) |
0 | GPIO25 | General-Purpose I/O | O | Hi-Z | Hi-Z | Hi-Z |
| 9 | GT_PWM02 | Pulse Width Modulated O/P | O | Hi-Z | |||||||||
| 2 | McAFSX | I2S Audio Port Frame Sync | O | Hi-Z | |||||||||
| See (6) | TCXO_EN | Enable to Optional External 40-MHz TCXO | O | O | |||||||||
| See (7) | SOP2 | Sense-On-Power 2 | I | ||||||||||
| 22 | WLAN_XTAL_N | WLAN Ana. | N/A | N/A | N/A | N/A | See (6) | WLAN_XTAL_N | 40-MHz XTAL Pulldown if ext TCXO is used. |
||||
| 23 | WLAN_XTAL_P | WLAN Ana. | N/A | N/A | N/A | N/A | WLAN_XTAL_P | 40-MHz XTAL or TCXO clock input | |||||
| 24 | VDD_PLL | Int. Pwr | N/A | N/A | N/A | N/A | VDD_PLL | Internal analog voltage | |||||
| 25 | LDO_IN2 | Int. Pwr | N/A | N/A | N/A | N/A | LDO_IN2 | Analog RF supply from ANA DC-DC output | |||||
| 26 | NC | WLAN Ana. | N/A | N/A | N/A | N/A | NC | Reserved | |||||
| 27 | NC | WLAN Ana. | N/A | N/A | N/A | N/A | NC | Reserved | |||||
| 28 | NC | WLAN Ana. | N/A | N/A | N/A | N/A | NC | Reserved | |||||
| 29(8) | ANTSEL1 | O Only | No | User config not required (9) |
No | GPIO_PAD_CONFIG_26 (0x4402 E108) |
0 | ANTSEL1(3) | Antenna Selection Control | O | Hi-Z | Hi-Z | Hi-Z |
| 30(8) | ANTSEL2 | O Only | No | User config not required (9) |
No | GPIO_PAD_CONFIG_27 (0x4402 E10C) |
0 | ANTSEL2(3) | Antenna Selection Control | O | Hi-Z | Hi-Z | Hi-Z |
| 31 | RF_BG | WLAN Ana. | N/A | N/A | N/A | N/A | RF_BG | RF BG band | |||||
| 32 | nRESET | Glob. Rst | N/A | N/A | N/A | N/A | nRESET | Master chip reset. Active low. | |||||
| 33 | VDD_PA_IN | Int. Pwr | N/A | N/A | N/A | N/A | VDD_PA_IN | PA supply voltage from PA DC-DC output. | |||||
| 34(5) | SOP1 | Config Sense | N/A | N/A | N/A | N/A | SOP1 | Sense On Power 1 | |||||
| 35(5) | SOP0 | Config Sense | N/A | N/A | N/A | N/A | SOP0 | Sense On Power 0 | |||||
| 36 | LDO_IN1 | Internal Power | N/A | N/A | N/A | N/A | LDO_IN1 | Analog RF supply from ana DC-DC output | |||||
| 37 | VIN_DCDC_ANA | Supply Input | N/A | N/A | N/A | N/A | VIN_DCDC_ANA | Analog DC-DC input (connected to chip input supply [VBAT]) | |||||
| 38 | DCDC_ANA_SW | Internal Power | N/A | N/A | N/A | N/A | DCDC_ANA_SW | Analog DC-DC switching node. | |||||
| 39 | VIN_DCDC_PA | Supply Input | N/A | N/A | N/A | N/A | VIN_DCDC_PA | PA DC-DC input (connected to chip input supply [VBAT]) | |||||
| 40 | DCDC_PA_SW_P | Internal Power | N/A | N/A | N/A | N/A | DCDC_PA_SW_P | PA DCDC switching node | |||||
| 41 | DCDC_PA_SW_N | Internal Power | N/A | N/A | N/A | N/A | DCDC_PA_SW_N | PA DCDC switching node | |||||
| 42 | DCDC_PA_OUT | Internal Power | N/A | N/A | N/A | N/A | DCDC_PA_OUT | PA buck converter output | |||||
| 43 | DCDC_DIG_SW | Internal Power | N/A | N/A | N/A | N/A | DCDC_DIG_SW | DIG DC-DC switching node | |||||
| 44 | VIN_DCDC_DIG | Supply Input | N/A | N/A | N/A | N/A | VIN_DCDC_DIG | DIG DC-DC input (connected to chip input supply [VBAT]) | |||||
| 45(10) | DCDC_ANA2_SW_P | I/O | No | User config not required (9)(11) |
No | GPIO_PAD_CONFIG_31 (0x4402 E11C) |
0 | GPIO31 | General-Purpose I/O | I/O | Hi-Z | Hi-Z | Hi-Z |
| 9 | UART0_RX | UART0 RX Data | I | ||||||||||
| 12 | McAFSX | I2S Audio Port Frame Sync | O | ||||||||||
| 2 | UART1_RX | UART1 RX Data | I | ||||||||||
| 6 | McAXR0 | I2S Audio Port Data 0 (RX/TX) | I/O | ||||||||||
| 7 | GSPI_CLK | General SPI Clock | I/O | ||||||||||
| See (6) | DCDC_ANA2_SW_P | ANA2 DCDC Converter +ve Switching Node. | |||||||||||
| 46 | DCDC_ANA2_SW_N | Internal Power | N/A | N/A | N/A | N/A | N/A | DCDC_ANA2_SW_N | ANA2 DCDC Converter -ve Switching Node. | ||||
| 47 | VDD_ANA2 | Internal Power | N/A | N/A | N/A | N/A | N/A | VDD_ANA2 | ANA2 DCDC O | ||||
| 48 | VDD_ANA1 | Internal Power | N/A | N/A | N/A | N/A | N/A | VDD_ANA1 | Analog supply fed by ANA2 DCDC output | ||||
| 49 | VDD_RAM | Internal Power | N/A | N/A | N/A | N/A | N/A | VDD_RAM | SRAM LDO output | ||||
| 50 | GPIO0 | I/O | No | User config not required (9) |
No | GPIO_PAD_CONFIG_0 (0x4402 E0A0) |
0 | GPIO0 | General-Purpose I/O | I/O | Hi-Z | Hi-Z | Hi-Z |
| 12 | UART0_CTS | UART0 Clear To Send Input (Active Low) | I | Hi-Z | Hi-Z | Hi-Z | |||||||
| 6 | McAXR1 | I2S Audio Port Data 1 (RX/TX) | I/O | Hi-Z | |||||||||
| 7 | GT_CCP00 | Timer Capture Port | I | Hi-Z | |||||||||
| 9 | GSPI_CS | General SPI Chip Select | I/O | Hi-Z | |||||||||
| 10 | UART1_RTS | UART1 Request To Send O (Active Low) | O | 1 | |||||||||
| 3 | UART0_RTS | UART0 Request To Send O (Active Low) | O | 1 | |||||||||
| 4 | McAXR0 | I2S Audio Port Data 0 (RX/TX) | I/O | Hi-Z | |||||||||
| 51 | RTC_XTAL_P | RTC Clock | N/A | N/A | N/A | N/A | RTC_XTAL_P | Connect 32.768-kHz XTAL or Froce external CMOS level clock | |||||
| 52(10) | RTC_XTAL_N | O Only | User config not required (9)(12) |
No | GPIO_PAD_CONFIG_32 (0x4402 E120) |
RTC_XTAL_N | Connect 32.768-kHz XTAL or connect a 100 kΩ to Vsupply. | Hi-Z | Hi-Z | ||||
| 0 | GPIO32 | General-Purpose I/O | I/O | Hi-Z | |||||||||
| 2 | McACLK | I2S Audio Port Clock O | O | Hi-Z | |||||||||
| 4 | McAXR0 | I2S Audio Port Data (Only O Mode Supported On Pin 52) | O | Hi-Z | |||||||||
| 6 | UART0_RTS | UART0 Request To Send O (Active Low) | O | 1 | |||||||||
| 8 | GSPI_MOSI | General SPI MOSI | I/O | Hi-Z | |||||||||
| 53 | GPIO30 | I/O | No | User config not required (9) |
No | GPIO_PAD_CONFIG_30 (0x4402 E118) |
0 | GPIO30 | General-Purpose I/O | I/O | Hi-Z | Hi-Z | Hi-Z |
| 9 | UART0_TX | UART0 TX Data | O | 1 | |||||||||
| 2 | McACLK | I2S Audio Port Clock O | O | Hi-Z | |||||||||
| 3 | McAFSX | I2S Audio Port Frame Sync | O | Hi-Z | |||||||||
| 4 | GT_CCP05 | Timer Capture Port | I | Hi-Z | |||||||||
| 7 | GSPI_MISO | General SPI MISO | I/O | Hi-Z | |||||||||
| 54 | VIN_IO2 | Supply Input | N/A | N/A | N/A | N/A | VIN_IO2 | Chip Supply Voltage (VBAT) | |||||
| 55 | GPIO1 | I/O | No | No | No | GPIO_PAD_CONFIG_1 (0x4402 E0A4) |
0 | GPIO1 | General-Purpose I/O | I/O | Hi-Z | Hi-Z | Hi-Z |
| 3 | UART0_TX | UART0 TX Data | O | 1 | |||||||||
| 4 | pCLK (PIXCLK) | Pixel Clock From Parallel Camera Sensor | I | Hi-Z | |||||||||
| 6 | UART1_TX | UART1 TX Data | O | 1 | |||||||||
| 7 | GT_CCP01 | Timer Capture Port | I | Hi-Z | |||||||||
| 56 | VDD_DIG2 | Internal Power | N/A | N/A | N/A | N/A | VDD_DIG2 | Internal Digital Core Voltage | |||||
| 57(13) | GPIO2 | Analog Input (up to 1.5 V)/ Digital I/O | Wake-Up Source | See (10)(14) | No | GPIO_PAD_CONFIG_2 (0x4402 E0A8) |
See (6) | ADC_CH0 | ADC Channel 0 Input (1.5V max) | I | Hi-Z | Hi-Z | |
| 0 | GPIO2 | General-Purpose I/O | I/O | Hi-Z | |||||||||
| 3 | UART0_RX | UART0 RX Data | I | Hi-Z | |||||||||
| 6 | UART1_RX | UART1 RXt Data | I | Hi-Z | |||||||||
| 7 | GT_CCP02 | Timer Capture Port | I | Hi-Z | |||||||||
| 58(13) | GPIO3 | Analog Input (up to 1.5V)/Digital I/O. | No | See (10)(14) | No | GPIO_PAD_CONFIG_3 (0x4402 E0AC) |
See (6) | ADC_CH1 | ADC Channel 1 Input (1.5V max) | I | Hi-Z | Hi-Z | |
| 0 | GPIO3 | General-Purpose I/O | I/O | Hi-Z | |||||||||
| 6 | UART1_TX | UART1 TX Data | O | 1 | |||||||||
| 4 | pDATA7 (CAM_D3) | Parallel Camera Data Bit 3 | I | Hi-Z | |||||||||
| 59(13) | GPIO4 | Analog Input (up to 1.5V)/Digital I/O. | Wake-up Source | See (10)(14) | No | GPIO_PAD_CONFIG_4 (0x4402 E0B0) |
See (6) | ADC_CH2 | ADC Channel 2 Input (1.5V max) | I | Hi-Z | Hi-Z | |
| 0 | GPIO4 | General-Purpose I/O | I/O | Hi-Z | |||||||||
| 6 | UART1_RX | UART1 RX Data | I | Hi-Z | |||||||||
| 4 | pDATA6 (CAM_D2) | Parallel Camera Data Bit 2 | I | Hi-Z | |||||||||
| 60(13) | GPIO5 | Analog Input (up to 1.5V)/Digital I/O. | No | See (10)(14) | No | GPIO_PAD_CONFIG_5 (0x4402 E0B4) |
See (6) | ADC_CH3 | ADC Channel 3 Input (1.5V max) | I | Hi-Z | Hi-Z | |
| 0 | GPIO5 | General-Purpose I/O | I/O | Hi-Z | |||||||||
| 4 | pDATA5 (CAM_D1) | Parallel Camera Data Bit 1 | I | Hi-Z | |||||||||
| 6 | McAXR1 | I2S Audio Port Data 1 (RX/TX) | I/O | Hi-Z | |||||||||
| 7 | GT_CCP05 | Timer Capture Port | I | Hi-Z | |||||||||
| 61 | GPIO6 | No | No | No | No | GPIO_PAD_CONFIG_6 (0x4402 E0B8) |
0 | GPIO6 | General-Purpose I/O | I/O | Hi-Z | Hi-Z | Hi-Z |
| 5 | UART0_RTS | UART0 Request To Send O (Active Low) | O | 1 | |||||||||
| 4 | pDATA4 (CAM_D0) | Parallel Camera Data Bit 0 | I | Hi-Z | |||||||||
| 3 | UART1_CTS | UART1 Clear To Send Input (Active Low) | I | Hi-Z | |||||||||
| 6 | UART0_CTS | UART0 Clear To Send Input (Active Low) | I | Hi-Z | |||||||||
| 7 | GT_CCP06 | Timer Capture Port | I | Hi-Z | |||||||||
| 62 | GPIO7 | I/O | No | No | No | GPIO_PAD_CONFIG_7 (0x4402 E0BC) |
0 | GPIO7 | General-Purpose I/O | I/O | Hi-Z | Hi-Z | Hi-Z |
| 13 | McACLKX | I2S Audio Port Clock O | O | Hi-Z | |||||||||
| 3 | UART1_RTS | UART1 Request To Send O (Active Low) | O | 1 | |||||||||
| 10 | UART0_RTS | UART0 Request To Send O (Active Low) | O | 1 | |||||||||
| 11 | UART0_TX | UART0 TX Data | O | 1 | |||||||||
| 63 | GPIO8 | I/O | No | No | No | GPIO_PAD_CONFIG_8 (0x4402 E0C0) |
0 | GPIO8 | General-Purpose I/O | I/O | Hi-Z | Hi-Z | Hi-Z |
| 6 | SDCARD_IRQ | Interrupt from SD Card (Future support) | I | ||||||||||
| 7 | McAFSX | I2S Audio Port Frame Sync | O | ||||||||||
| 12 | GT_CCP06 | Timer Capture Port | I | ||||||||||
| 64 | GPIO9 | I/O | No | No | No | GPIO_PAD_CONFIG_9 (0x4402 E0C4) |
0 | GPIO9 | General-Purpose I/O | I/O | Hi-Z | Hi-Z | Hi-Z |
| 3 | GT_PWM05 | Pulse Width Modulated O/P | O | ||||||||||
| 6 | SDCARD_DATA | SD Cad Data | I/O | ||||||||||
| 7 | McAXR0 | I2S Audio Port Data (Rx/Tx) | I/O | ||||||||||
| 12 | GT_CCP00 | Timer Capture Port | I | ||||||||||
| 65 | GND_TAB | Thermal pad and electrical ground | |||||||||||
Figure 3-2 Board Configuration to Use Pins 45 and 52 as Digital Signals
All unused pins must be left as no connect (NC) pins. For a list of NC pins, see Table 3-2.
| FUNCTION | SIGNAL NAME | PIN NUMBER |
|---|---|---|
| WLAN Analog | NC | 26 |
| WLAN Analog | NC | 27 |
| WLAN Analog | NC | 28 |
Table 3-3 lists the recommended pin multiplexing configurations.
| CC3200 Recommended Pinout Grouping Use – Examples(2) | |||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|
| Home Security High-end Toys | Wifi Audio ++ Industrial | Sensor-Tag | Home Security Toys | Wifi Audio ++ Industrial | WiFi Remote w/ 7x7 keypad and audio | Sensor Door-Lock Fire-Alarm Toys w/o Cam | Industrial Home Appliances | Industrial Home Appliances Smart-Plug | Industrial Home Appliances" | GPIOs | |
| External 32 kHz(1) | External 32 kHz (1) | External TCXO 40 MHZ (-40 to +85°C) | |||||||||
| Cam + I2S (Tx or Rx) + I2C + SPI + SWD + UART-Tx + (App Logger) 2 GPIO + 1PWM + *4 overlaid wakeup from Hib | I2S (Tx & Rx) + 1 Ch ADC + 1x 4wire UART + 1x 2wire UART + 1bit SD Card + SPI + I2C + SWD + 3 GPIO + 1 PWM + 1 GPIO with Wake-From-Hib | I2S (Tx & Rx) + 2 Ch ADC + 2wire UART + SPI + I2C + SWD + 2 PMW + 6 GPIO + 3 GPIO with Wake-From-Hib | Cam + I2S (Tx or Rx) + I2C + SWD + UART-Tx + (App Logger) 4 GPIO + 1PWM + *4 overlaid wakeup from HIB | I2S (Tx & Rx) + 1 Ch ADC + 2x 2wire UART + 1bit SD Card + SPI + I2C + SWD + 4 GPIO + 1 PWM + 1 GPIO with Wake-From-Hib | I2S (Tx & Rx) + 1 Ch ADC + UART (Tx Only) I2C + SWD + 15 GPIO + 1 PWM + 1 GPIO with Wake-From-Hib | I2S (Tx or Rx) + 2 Ch ADC + 2 wire UART + SPI + I2C + 3 PMW + 3 GPIO with Wake-From-Hib + 5 GPIO SWD + | 4 Ch ADC + 1x 4wire UART + 1x 2wire UART + SPI + I2C + SWD + 1 PWM + 6 GPIO + 1 GPIO with Wake-From-Hib Enable for Ext 40 MHz TCXO | 3 Ch ADC + 2wire UART + SPI + I2C + SWD + 3 PWM + 9 GPIO + 2 GPIO with Wake-From-Hib | 2 Ch ADC + 2wire UART + I2C + SWD + 3 PWM + 11 GPIO + 5 GPIO with Wake-From-Hib | ||
| Pin Number | Pinout #11 | Pinout #10 | Pinout #9 | Pinout #8 | Pinout #7 | Pinout #6 | Pinout #5 | Pinout #4 | Pinout #3 | Pinout #2 | Pinout #1 |
| 52 | GSPI-MOSI | McASP-D0 (Tx) | GPIO_32 output only | ||||||||
| 53 | GSPI-MISO | MCASP-ACLKX | MCASP-ACLKX | GPIO_30 | GPIO_30 | GPIO_30 | GPIO_30 | UART0-TX | GPIO_30 | UART0-TX | GPIO_30 |
| 45 | GSPI-CLK | McASP-AFSX | McASP-D0 | GPIO_31 | McASP-AFSX | McASP-AFSX | McASP-AFSX | UART0-RX | GPIO_31 | UART0-RX | GPIO_31 |
| 50 | GSPI-CS | McASP-D1 (Rx) | McASP-D1 | McASP-D1 | McASP-D1 | McASP-D1 | McASP-D1 | UART0-CTS | GPIO_0 | GPIO_0 | GPIO_0 |
| 55 | pCLK (PIXCLK) | UART0-TX | UART0-TX | PIXCLK | UART0-TX | UART0-TX | UART0-TX | GPIO-1 | UART0-TX | GPIO_1 | GPIO_1 |
| 57 | (wake) GPIO2 | UART0-RX | UART0-RX | (wake) GPIO2 | UART0-RX | GPIO_2 | UART0-RX | ADC-0 | UART0-RX | (wake) GPIO_2 | (wake) GPIO_2 |
| 58 | pDATA7 (D3) | UART1-TX | ADC-CH1 | pDATA7 (D3) | UART1-TX | GPIO_3 | ADC-1 | ADC-1 | ADC-1 | ADC-1 | GPIO_3 |
| 59 | pDATA6 (D2) | UART1-RX | (wake) GPIO_4 | pDATA6 (D2) | UART1-RX | GPIO_4 | (wake) GPIO_4 | ADC-2 | ADC-2 | (wake) GPIO_4 | (wake) GPIO_4 |
| 60 | pDATA5 (D1) | ADC-3 | ADC-3 | pDATA5 (D1) | ADC-3 | ADC-3 | ADC-3 | ADC-3 | ADC-3 | ADC-3 | GPIO_5 |
| 61 | pDATA4 (D0) | UART1-CTS | GPIO_6 | pDATA4 (D0) | GPIO_6 | GPIO_6 | GPIO_6 | UART0-RTS | GPIO_6 | GPIO_6 | GPIO_6 |
| 62 | McASP-ACLKX | UART1-RTS | GPIO_7 | McASP-ACLKX | McASP-ACLKX | McASP-ACLKX | McASP-ACLKX | GPIO_7 | GPIO_7 | GPIO_7 | GPIO_7 |
| 63 | McASP-AFSX | SDCARD-IRQ | McASP-AFSX | McASP-AFSX | SDCARD-IRQ | GPIO_8 | GPIO_8 | GPIO_8 | GPIO_8 | GPIO_8 | GPIO_8 |
| 64 | McASP-D0 | SDCARD-DATA | GT_PWM5 | McASP-D0 | SDCARD-DATA | GPIO_9 | GT_PWM5 | GT_PWM5 | GT_PWM5 | GT_PWM5 | GPIO_9 |
| 1 | UART1-TX | SDCARD-CLK | GPIO_10 | UART1-TX | SDCARD-CLK | GPIO_10 | GT_PWM6 | UART1-TX | GT_PWM6 | GPIO_10 | GPIO_10 |
| 2 | (wake) pXCLK (XVCLK) | SDCARD-CMD | (wake) GPIO_11 | (wake) pXCLK (XVCLK) | SDCARD-CMD | GPIO_11 | (wake) GPIO_11 | UART1-RX | (wake) GPIO_11 | (wake) GPIO_11 | (wake) GPIO_11 |
| 3 | pVS (VSYNC) | I2C-SCL | I2C-SCL | pVS (VSYNC) | I2C-SCL | GPIO_12 | I2C-SCL | I2C-SCL | I2C-SCL | GPIO_12 | GPIO_12 |
| 4 | (wake) pHS (HSYNC) | I2C-SDA | I2C-SDA | (wake) pHS (HSYNC) | I2C-SDA | GPIO_13 | I2C-SDA | I2C-SDA | I2C-SDA | (wake) GPIO_13 | (wake) GPIO_13 |
| 5 | pDATA8 (D4) | GSPI-CLK | GSPI-CLK | pDATA8 (D4) | GSPI-CLK | I2C-SCL | GSPI-CLK | GSPI-CLK | GSPI-CLK | I2C-SCL | GPIO_14 |
| 6 | pDATA9 (D5) | GSPI-MISO | GSPI-MISO | pDATA9 (D5) | GSPI-MISO | I2C-SDA | GSPI-MISO | GSPI-MISO | GSPI-MISO | I2C-SDA | GPIO_15 |
| 7 | pDATA10 (D6) | GSPI-MOSI | GSPI-MOSI | pDATA10 (D6) | GSPI-MOSI | GPIO_16 | GSPI-MOSI | GSPI-MOSI | GSPI-MOSI | GPIO_16 | GPIO_16 |
| 8 | (wake) pDATA11 (D7) | GSPI-CS | GSPI-CS | (wake) pDATA11 (D7) | GSPI-CS | GPIO_17 | GSPI-CS | GSPI-CS | GSPI-CS | (wake) GPIO_17 | (wake) GPIO_17 |
| 11 | SPI-FLASH_CLK | SPI-FLASH_CLK | SPI-FLASH_CLK | SPI-FLASH_CLK | SPI-FLASH_CLK | SPI-FLASH_CLK | SPI-FLASH_CLK | SPI-FLASH_CLK | SPI-FLASH_CLK | SPI-FLASH_CLK | SPI-FLASH_CLK |
| 12 | SPI-FLASH-DOUT | SPI-FLASH-DOUT | SPI-FLASH-DOUT | SPI-FLASH-DOUT | SPI-FLASH-DOUT | SPI-FLASH-DOUT | SPI-FLASH-DOUT | SPI-FLASH-DOUT | SPI-FLASH-DOUT | SPI-FLASH-DOUT | SPI-FLASH-DOUT |
| 13 | SPI-FLASH-DIN | SPI-FLASH-DIN | SPI-FLASH-DIN | SPI-FLASH-DIN | SPI-FLASH-DIN | SPI-FLASH-DIN | SPI-FLASH-DIN | SPI-FLASH-DIN | SPI-FLASH-DIN | SPI-FLASH-DIN | SPI-FLASH-DIN |
| 14 | SPI-FLASH-CS | SPI-FLASH-CS | SPI-FLASH-CS | SPI-FLASH-CS | SPI-FLASH-CS | SPI-FLASH-CS | SPI-FLASH-CS | SPI-FLASH-CS | SPI-FLASH-CS | SPI-FLASH-CS | SPI-FLASH-CS |
| 15 | GPIO_22 | GPIO_22 | GPIO_22 | GPIO_22 | GPIO_22 | GPIO_22 | GPIO_22 | GPIO_22 | GPIO_22 | GPIO_22 | GPIO_22 |
| 16 | I2C-SCL | GPIO_23 | GPIO_23 | I2C-SCL | GPIO_23 | GPIO_23 | GPIO_23 | GPIO_23 | GPIO_23 | GPIO_23 | GPIO_23 |
| 17 | I2C-SDA | (wake) GPIO_24 | (wake) GPIO_24 | I2C-SDA | (wake) GPIO_24 | (wake) GPIO_24 | (wake) GPIO_24 | (wake) GPIO_24 | (wake) GPIO_24 | GT-PWM0 | (wake) GPIO_24 |
| 19 | SWD-TCK | SWD-TCK | SWD-TCK | SWD-TCK | SWD-TCK | SWD-TCK | SWD-TCK | SWD-TCK | SWD-TCK | SWD-TCK | SWD-TCK |
| 20 | SWD-TMS | SWD-TMS | SWD-TMS | SWD-TMS | SWD-TMS | SWD-TMS | SWD-TMS | SWD-TMS | SWD-TMS | SWD-TMS | SWD-TMS |
| 18 | GPIO_28 | GPIO_28 | GPIO_28 | GPIO_28 | GPIO_28 | GPIO_28 | GPIO_28 | GPIO_28 | GPIO_28 | GPIO_28 | GPIO_28 |
| 21 | GT_PWM2 | GT_PWM2 | GT_PWM2 | GT_PWM2 | GT_PWM2 | GT_PWM2 | GT_PWM2 | TCXO_EN | GT_PWM2 | GT_PWM2 | GPIO_25 out only |
Table 3-4 describes the use, drive strength, and default state of these pins at first-time power up and reset (nRESET pulled low).
| Pin | Board Level Configuration and Use | Default State at First Power Up or Forced Reset | State after Configuration of Analog Switches (ACTIVE, LPDS, and HIB Power Modes) | Maximum Effective Drive Strength (mA) |
|---|---|---|---|---|
| 29 | Connected to the enable pin of the RF switch (ANTSEL1). Other use not recommended. | Analog is isolated. The digital I/O cell is also isolated. | Determined by the I/O state, as are other digital I/Os. | 4 |
| 30 | Connected to the enable pin of the RF switch (ANTSEL2). Other use not recommended. | Analog is isolated. The digital I/O cell is also isolated. | Determined by the I/O state, as are other digital I/Os. | 4 |
| 45 | VDD_ANA2 (pin 47) must be shorted to the input supply rail. Otherwise, the pin is driven by the ANA2 DC-DC. | Analog is isolated. The digital I/O cell is also isolated. | Determined by the I/O state, as are other digital I/Os. | 4 |
| 50 | Generic I/O | Analog is isolated. The digital I/O cell is also isolated. | Determined by the I/O state, as are other digital I/Os. | 4 |
| 52 | The pin must have an external pullup of 100 K to the supply rail and must be used in output signals only. | Analog is isolated. The digital I/O cell is also isolated. | Determined by the I/O state, as are other digital I/Os. | 4 |
| 53 | Generic I/O | Analog is isolated. The digital I/O cell is also isolated. | Determined by the I/O state, as are other digital I/Os. | 4 |
| 57 | Analog signal (1.8 V absolute, 1.46 V full scale) | ADC is isolated. The digital I/O cell is also isolated. | Determined by the I/O state, as are other digital I/Os. | 4 |
| 58 | Analog signal (1.8 V absolute, 1.46 V full scale) | ADC is isolated. The digital I/O cell is also isolated. | Determined by the I/O state, as are other digital I/Os. | 4 |
| 59 | Analog signal (1.8 V absolute, 1.46 V full scale) | ADC is isolated. The digital I/O cell is also isolated. | Determined by the I/O state, as are other digital I/Os. | 4 |
| 60 | Analog signal (1.8 V absolute, 1.46 V full scale) | ADC is isolated. The digital I/O cell is also isolated. | Determined by the I/O state, as are other digital I/Os. | 4 |
When a stable power is applied to the CC3200 chip for the first time or when supply voltage is restored to the proper value following a prior period with supply voltage below 1.5 V, the level of the digital pads are undefined in the period starting from the release of nRESET and until DIG_DCDC powers up. This period is less than approximately 10 ms. During this period, pads can be internally pulled weakly in either direction. If a certain set of pins are required to have a definite value during this pre-reset period, an appropriate pullup or pulldown must be used at the board level. The recommended value of this external pull is 2.7 KΩ.