ZHCSJ06B November 2017 – September 2022 ADS7142-Q1
PRODUCTION DATA
The ADS7142-Q1 has two separate power supplies: AVDD and DVDD. The device operates on AVDD; DVDD is used for the interface circuits. AVDD and DVDD can be independently set to any value within the permissible ranges. The AVDD supply also defines the full-scale input range of the device. Always set the AVDD supply to be greater than or equal to the maximum input signal to avoid saturation of codes. Decouple the AVDD and DVDD pins respectively with CAVDD = 220 nF and CDVDD = 100 nF ceramic decoupling capacitors, as illustrated in Figure 8-9.
Figure 8-9 Power-Supply Decoupling