LP-MSPM0L2228 is a prototype evaluation module and is available in limited quantities.
LP-MSPM0L2228
MSPM0L2228 LaunchPad(TM) development kit for 32-MHz Arm(R) Cortex(R)-M0+ MCU
LP-MSPM0L2228
概述
The MSPM0L2228 LaunchPad™ development kit is an easy-to-use evaluation module for the MSPM0L2228 microcontroller (MCU). It contains everything needed to start developing on the MSPM0L2228 M0+ MCU platform, including on-board debug probe for programming, debugging and EnergyTrace technology. The board also features on-board buttons, LEDs, an RGB LED and a seven-segment LCD panel.
特性
- LCD screen to show LCD control
- RGB LEDs for PWMs
Arm Cortex-M0+ MCU
立即订购并开发
LP-MSPM0L2228 — MSPM0L2228 LaunchPad™ 开发套件
MSP-GANG-SOFTWARE — MSP-GANG 软件
MSP-GANG-SOFTWARE — MSP-GANG 软件
MSP-GANG Installer 1.03.09.00
产品
Arm Cortex-M0+ MCU
MSP430 微控制器
硬件开发
评估板
开发套件
文档
MSP-GANG Manifest
发布信息
The MSP Gang Programmer is a MSPM0/MSP430/MSP432 device programmer that can program up to eight identical flash or FRAM devices at the same time. The MSP Gang Programmer connects to a host PC using a standard RS-232 or USB connection and provides flexible programming options that allow the user to fully customize the process.
The MSP Gang Programmer is provided with an expansion board, called the Gang Splitter, that implements the interconnections between the MSP Gang Programmer and multiple target devices. Eight cables are provided that connect the expansion board to eight target devices (via JTAG or Spy-Bi-Wire connectors). The programming can be done with a PC or as a standalone device. A PC-side Graphical User Interface is also available and is DLL-based.
Features:
- Quickly and reliably program Flash or FRAM-based MSP devices via an RS-232 or USB interface
- Several programming modes:
- Interactive Mode Programming while connected to PC using the MSP GANG Programmer GUI
- Program from Image: An image can be stored, which contains configuration options and code files. This allows users to program MSP devices standalone, without a PC
- Programming from Script: Enables developers to automate more complicated programming procedures.
- Intuitive GUI for configuring, programming and testing production setup
- SD Card slot for storing images
- LCD screen for easy programming without a PC
- Supports up to 8 targets simultaneously
- Supports MSPM0/MSP430/MSP432 devices
最新信息
- Added low-power mode debug support for MSPM0
MSPM0-SDK — MSPM0 Software Development Kit (SDK)
MSPM0 SDK for Windows
MSPM0 SDK for Linux
MSPM0 SDK for macOS
产品
Arm Cortex-M0+ MCU
硬件开发
评估板
文档
MSPM0 SDK Documentation Overview
MSPM0 SDK Manifest
发布信息
The MSPM0 SDK delivers components that enable engineers to develop applications on Texas Instruments MSPM0 microcontroller devices. The product is comprised of multiple software components and more than 150 examples of how to use these components together. In addition, examples are provided to demonstrate the use of each functional area and each supported device and as a starting point for your own projects.
The MSPM0 SDK includes support for FreeRTOS and a wide variety of middleware and drivers, including:
- Support for MSPM0L11xx/L13xx, MSPM0G1x0x/G3x0x, MSPM0C110x, MSPS003FX, and MSPM0L122X/L22X
- DriverLib with optimized footprint and performance
- Motor control examples for Stepper, Brushed, Sensorless FOC, and Hall Sensored Trap
- EEPROM emulation library
- IQMath for fixed point math
- Boot Image Manager to add secure booting features
- Libraries and demos for multiple protocols, including DALI, SMBus, PMBus, 1-Wire, etc.
- and more...
The MSPM0 MCU portfolio offers a single development environment that delivers flexible hardware, software and tool options for customers developing applications. A one-time investment with the MSPM0 software development kit (SDK) allows you create portable and modular code, opening the door to create unlimited applications.
最新信息
- Handled MSPM0C110X ADC errata with new ADC and FactoryRegion DriverLib APIs
- Fixed variety of Timer DriverLib API bugs
- Updated SysConfig TIMER modules with improvements and fixes for channel configuration
- Updated Sensorless FOC BLDC Motor Control Library with bug fixes and new features
- Updated FlashCTL DriverLib APIs with improvements
- Added documentation for OpenOCD support for MSPM0
- Refer to the Release Notes for more details
CCSTUDIO-THEIA — Code Composer Studio™ integrated development environment (IDE) Theia
CCSTUDIO-THEIA — Code Composer Studio™ integrated development environment (IDE) Theia
Link to Windows single file (offline) installer for Code Composer Studio Theia for production use with MSPM0 and MSP430 devices and evaluation for all other families.
Link to Linux single file (offline) installer for Code Composer Studio Theia for production use with MSPM0 and MSP430 devices and evaluation for all other families.
Link to OS X single file (offline) installer for Code Composer Studio Theia for production use with MSPM0 and MSP430 devices and evaluation for all other families.
产品
Arm Cortex-M0+ MCU
Sub-1GHz 无线 MCU
汽车类无线连接产品
低功耗 2.4GHz 产品
其他无线产品
MSP430 微控制器
C2000 实时微控制器
Arm Cortex-R MCU
基于 Arm 的处理器
汽车毫米波雷达传感器
工业毫米波雷达传感器
硬件开发
评估板
发布信息
Bug Fixes
- XDS110 serial number could be corrupted on a split launchpad
- Many build and project system related improvements.
Known Issues
- Decoding of core trace data may take up to 20 seconds for large captures. Performance can be improved 2x - 3x by performing the following actions:
- Right click on the core and select "Show all cores" from the context menu
- Select the new visible node which is called "DebugCell_TBR_0"
- Right click on that node and select "Connect Target"
- PC Hibernation affects CCS Theia inter-process communication with Resource Explorer opened. You may see a message “Error communicating with Cloud Agent “. Also, a notification panel in bottom right will be shown indicating that CCS Theia has gone offline. Please choose Restart option to restart CCS Theia and re-establish IPC communication.
General Information
- New Theia-IDE based IDE:
- Simple, easy-to-use environment
- Compatible with VS Code® extensions:
- You may need to configure proxy settings to access open-vsx.org where Theia enabled extensions are hosted.
- Source code navigation.
- Debug views such as breakpoints, callstack, variables, registers, memory and graphs.
- Target Configuration View
- Project-less debug support
- New features are being added with every release, please check What’s New section for details.
Compatibility:
- Project System is fully compatible with existing Code Composer Studio projects, meaning that existing projects (or example projects in SDKs) can be imported into CCS Theia. Workspaces are not compatible.
- Simply import your existing projects or examples from the SDK and get started
- Debug: Project based debugging is supported by providing same single click Debug Active Project action as in CCS 12.x. Project-less debug, ability to start a debug session from target configuration file (ccxml) is supported.
- Workspace: CCS Theia is using different underlying framework as such workspaces are not compatible between CCS products based on Eclipse. However, projects are fully compatible.
- CCS Theia supports ability to open a folder that holds CCS Projects or open a folder where projects should reside.
- Similar to VS Code, CCS Theia can open multiple distinct folders that hold projects. This is documented in VS Code as multi-root workspace. However, project names need to be unique across different folders.
Compilers
- TI CLANG 3.2.2 LTS, C2800 Compiler Tools v22.6.1 and MSP430 Compiler Tools v21.6.1.LTS compilers are bundled
Device Support
- Recommended for production development: MSPM0, MSP430, Wireless connectivity, Sitara MCU, mmWave
- Evaluation, not recommended for production development: Sitara MPU, Jacinto
最新信息
- Update to Theia v1.46 baseline
- Improvements in trace support
- Energy Trace ++ support for MSP430
- System Project debug with OptiShare
- Breakpoint view improvements
- Register view improvements
- Real time view updates
- MSPM0 Wait-in-reset support
- ARM Core Trace
MSPM0-ANALOG-CONFIGURATOR — Analog Configurator for MSPM0
MSPM0 Analog Configurator in TI Gallery
产品
Arm Cortex-M0+ MCU
硬件开发
评估板
发布信息
The MSPM0 Analog Configurator is a graphical configuration tool designed to simplify and accelerate the design and enablement of an analog signal chain using a MSPM0 device with no traditional coding development necessary.
The tool uses an intuitive GUI to configure a signal chain using the high analog integration of MSPM0 devices, analyze and plot signals in real-time, and generate the configuration and code necessary to flash the device.
The current release only supports MSPM0L and MSPM0G production samples. See this FAQ for more information about silicon differences.
Analog Configurator supports the following features:
- Drag&drop designer tab to add analog components
- Code generation of CCS projects and SysConfig files
- Graphical plotting capability
最新信息
- Support for MSPM0L and MSPM0G production samples
技术文档
类型 | 标题 | 下载最新的英文版本 | 日期 | |||
---|---|---|---|---|---|---|
* | EVM 用户指南 | LP-MSPM0L2228 Evaluation Module User's Guide | PDF | HTML | 2024年 5月 1日 | ||
证书 | LP-MSPM0L2228 EU Declaration of Conformity (DoC) | 2024年 4月 22日 |