TIDUEA0A March 2019 – September 2020
Heat Meters are commonly used for billing heat energy for residential users in multi-dwelling units across many countries, while Cooling Meters are often found in commercial, storage, or logistic buildings and industrial environments. Heat Meters and Cooling Meters are both thermal energy meters, as defined in Annex VI of the Measuring Instruments Directive (MID) 2014/32/EU(4) of the European Parliament and of the Council of 26 February 2014. The MID document is the harmonization of the laws of the member states related to creating a common market for measuring instruments across all countries of the EU. Cooling Meters are not part of the MID and are usually regulated nationally.
Thermal energy meters are basically regular flow meters, for example water meters, extended with a precise differential temperature measurement (DTM) subsystem to capture the temperature difference between the inlet and the outlet flow. If the medium temperature flow of the inlet is lower than the temperature of the outlet, then heat is being dissipated, otherwise heat gets absorbed, which means this is a cooling system.
Heat Meters and Cooling Meters are therefore very similar. However, in order to be able to use both types for billing, a type examination certificate is required in each case. For a type examination certificate the requirements of EN 1434 must be fulfilled. Texas Instruments has a close cooperation with JUMO GmbH & Co. KG to fulfil these requirements and create a type examination certificate.