SWCU192 November 2021 CC1312R7 , CC1352P7 , CC2652P7 , CC2652R7
AUX_ANAIF:DACCTL.DAC_VOUT_SEL selects Reference DAC output connection:
Selection of only one output connection at a time is allowed. The user must ensure that the connected analog node only has one driver at all times. To avoid shorting signals together internally, TI provides ROM-based TI-DriverLib functions that ensure a break-before-make switching of the internal muxes.
The following subsections describe the different connections.