The AWR2944EVM can be connected to the
DCA1000 EVM platform to allow for LVDS data streaming. Figure 2-22 shows the AWR2944EVM interfaced to the DCA1000 EVM.
When using the AWR2944EVM with the
DCA1000 EVM, the following settings must be used.
- Set the AWR2944EVM to SOP2
mode.
- Set the
DCA1000 EVM switches to the following configuration.
- The 12-V supply must be connected
to J12 on the AWR2944EVM
- A 5-V supply must be connected to
J2 on the DCA1000 EVM
- A micro USB cable must be
connected to the FTDI port on the AWR2944EVM (J10)
- The Samtec ribbon cable must be
connected to J7 on the AWR2944EVM and J3 on the DCA1000 EVM
- An RJ45 cable must be connected
to J6 on the DCA1000 EVM