SPRUJ22A November 2021 – March 2023 AWR2944
J8 provides access to the onboard XDS110 (TM4C1294NCPDT) emulator. This connection provides the following interfaces to the PC:
When the J8 USB is connected to the PC the device manager should recognize two XDS110 COM ports under Ports (COM & LPT).
XDS110 debug probe and data port are detected under Texas Instruments Debug Probes.
If the PC is unable to recognize the above COM ports, install the latest EMUpack.