ZHCSEO6B DECEMBER 2012 – December 2015 TPS92560
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
In the applications that need true regulation of the LED current, the intrinsic input current control loop can be changed to monitor the LED current by adding an external LED current sensing circuit. Figure 18 and Figure 23 show the example circuits for true LED current regulation in boost and SEPIC configurations respectively. In the circuits, the U3 (TL431) maintains a constant 2.5-V voltage drop on the resistors, R3 and R7. Because the U2 (TL431) maintains a constant voltage drop on the R3, the power dissipation on the output current sensing resistor, R7 can be minimized by setting a low voltage drop on the R7. Because the change of the current flowing through the R7 reflects in the change of the cathode current of U3 and eventually adjusts the ADJ pin voltage of the TPS92560, the LED current is regulated independent of the change of the input voltage.
The specifications of the boost application circuit in Figure 18 are as listed as follows:
First choose a value for RADJ2 in the range of 1 kΩ and 10 kΩ. For this example RADJ2 = 1 kΩ is chosen. Then calculate RADJ1 for the desired OVP level using Equation 25.
Choose the nearest standard resistor value of RADJ1 = 102 kΩ.
Given the calculated ADJ resistor values the sense voltage (VSEN) can be calculated using Equation 26.
Given a current sense voltage of 206 mV the current sense resistor value (RSEN) can be calculated using Equation 27.
The nearest standard value if 0.412Ω so choose RSEN = 0.412Ω.
Given a desired switching frequency of 1.4 MHz the inductor value can be calculated using Equation 28.
Choose the closest standard inductor value of L = 22 µH.
The specifications of the boost application circuit in Figure 18 are as as follows:
All curves taken at VIN = 3 V to 18 VDC in boost configuration, with 300mA nominal output current, 6 serial LEDs. TA = 25°C.
The specifications of the SEPIC application circuit in Figure 18 are as listed as follows:
All curves taken at VIN = 3 V to 18 VDC in SEPIC configuration, with 300-mA nominal output current, 4 serial LEDs. TA = 25°C.