ZHCSEO6B DECEMBER 2012 – December 2015 TPS92560
PRODUCTION DATA.
The VP input capacitor and ADJ resistors/capacitor should be placed as close to the IC as possible. The VCC capacitor should also be placed close to the device. Minimize the switching node area (connection between Q1, L1, and D3) and keep the discontinuous current switching path as short as possible. This includes the loop formed by Q1, COUT, and the diode D3 (designated by the red arrows). The ground connections for the TPS92560 and RSEN should be tide closely together with a solid ground plane. The node connecting the SEN pin, SRC pin, the source of Q1, CVCC, and COUT should be small with all components connected closely together.