ZHCSBP7C October 2013 – December 2018 TPS24750 , TPS24751
UNLESS OTHERWISE NOTED, this document contains PRODUCTION DATA.
A resistor connected from this pin to GND scales the current-limit and power-limit settings, as illustrated in the Functional Block Diagram. The voltage present at this pin is proportional to the current flowing through sense resistor RSENSE. This voltage can be used as a means of monitoring current flow through the system. The value of RIMON can be calculated from Equation 3. This pin must not have a bypass capacitor or any other load except for RIMON.