ZHCSHW5A September 2017 – December 2017 TPS23521
PRODUCTION DATA.
Timer is a critical feature in the hot swap, which manages the stress level in the MOSFET. The timer will source and sink current into the timer capacitor as follows:
The TPS23521 times out and shuts down the hot swap as follows.
The above behavior maximizes the ability of the hot swap to ride out voltage steps, while ensuring that the FET remains safe even if the part can not ride out a voltage step.
A cool down period follows after the part times out. During this time the timer performs the following:
The part attempts to restart after finishing the above. If the UVEN signal is toggled while the 64 cycles are in progress the part restarts immediately after the 64 cycles are completed.
The timer operates as follows when recovering from POR:
The Time Out (TTO) can be computed using the equations below. Note that the time out depends on the VDS of the MOSFET.