ZHCSP56 September 2023 TPS1HTC30-Q1
PRODUCTION DATA
Method 1: Blocking diode connected with VS. Both the device and load are protected when in reverse polarity.
Method 2 (GND network protection): Only the high-side device is protected under this connection. The load reverse loop is limited by the load itself. Note when reverse polarity happens, the continuous reverse current through the power FET must be less than Irev. Of the three types of ground pin networks, TI strongly recommends type 3 (the resistor and diode in parallel). No matter what types of connection are between the device GND and the board GND, if a GND voltage shift happens, make sure the following proper connections for the normal operation:
where
If multiple high-side power switches are used, the resistor can be shared among devices.