ZHCSJK2O October 2004 – September 2023 PCA9306
PRODUCTION DATA
The resistor is used to limit the current between VREF2 and VREF1 (denoted as RCC) and helps to establish the reference voltage on the enable pin. The 200k resistor can be changed to a lower value; however, the bias current proportionally increases as the resistor decreases.
where
Keep in mind RCC should not be sized low enough that ICC exceeds the absolute maximum continuous channel current specified in section 6.1 which is described in Equation 6.
where