ZHCSHU9K September 2011 – December 2023 LMK03806
PRODUCTION DATA
The RESET bit is located in register R0 only. Setting this bit will cause the silicon default values to be loaded. When programming register R0 with the RESET bit set, all other programmed values are ignored. After resetting the device, the register R0 must be programmed again (with RESET = 0) to set non-default values in register R0.
The reset occurs on the falling edge of the LEuWire pin which loaded R0 with RESET = 1.
The RESET bit is automatically cleared upon writing any other register. For instance, when R0 is written to again with default values.
R0[17] | STATE |
---|---|
0 | Normal operation |
1 | Reset (automatically cleared) |