ZHCSEN6D October 2014 – February 2022 DS90UH948-Q1
PRODUCTION DATA
When designing the transmission channel, consider the total insertion loss of all components in the signal path between a serializer and a deserializer. An example of the transmission channel connects from a FPD-Link serializer (SER) to a deserializer would consist of a serializer PCB, two or more connectors, one or more cables, and a deserializer PCB as shown in #T5552880-12
Table 7-6 depicts the maximum attenuation using DS90UH948-Q1. The PCLK is the maximum frequency based on the channel attenuation. The attenuation increases with cable length and frequency. The trace length of the PCB has very small contribution to the differential insertion loss of the transmission channel. Table 7-6 shows the maximum attenuation that the AEQ can compensate for at the given PCLK and resultant Nuyquist frequency.
PCLK (MHz) | FPD-LINK LINE RATE (Gbps) | NYQUIST FREQUENCY (GHz) | CHANNEL ATTENUATION (dB) | TYP CABLE LENGTH (m) |
---|---|---|---|---|
170 | 2.97 | 1.48 | -15 | 10 |
188 | 3.29 | 1.64 | -12 | 7 |
192 | 3.36 | 1.68 | -9 | 5 |