ZHCSEA7A June 2015 – September 2015 CDCEL824
PRODUCTION DATA.
There is no restriction on the power-up sequence. In case VDDOUT is applied first, it is recommended to ground VDD. In case VDDOUT is powered while VDD is floating, there is a risk of high current flowing on the VDDOUT.
The device has a power-up control that is connected to the 1.8-V supply. This keeps the whole device disabled until the 1.8-V supply reaches a sufficient voltage level. Then the device switches on all internal components, including the outputs. If there is a VDDOUT available before the VDD supply, the outputs will stay disabled until the VDD supply has reached a certain level.