选择版本

选择版本

未找到结果。请清除搜索,并重试。

PROCESSOR-SDK-LINUX-AM57X

适用于 AM57x 的 Linux 处理器 SDK

选择版本
未找到结果。请清除搜索,并重试。
版本: 05.03.00.07
发布日期: 05 四月 2019

Code Composer Studio IDE for Windows Host

Code Composer Studio IDE for Linux Host

AM57xx Pin Mux Configuration Utility

Only used when creating an SD Card on Windows

MD5 校验和

Standalone Linaro Toolchain - Linaro GCC 7.2.1 2017.11 hard-float toolchain

AM57xx Linux SDK prebuilt BSP binaries and root filesystem

MD5 校验和

AM57xx Linux SDK Arago source downloads

MD5 校验和

Quick Start Guide that was included in the EVM kit

产品
基于 Arm 的处理器
AM5706 Sitara 处理器:成本经优化的 Arm Cortex-A15 和 DSP 以及安全引导 AM5708 Sitara 处理器:成本经优化的 Arm Cortex-A15 和 DSP、多媒体和安全引导 AM5716 Sitara 处理器: Arm Cortex-A15 和 DSP AM5718 Sitara 处理器: Arm Cortex-A15 和 DSP、多媒体 AM5726 Sitara 处理器:双核 Arm Cortex-A15 和双核 DSP AM5728 Sitara 处理器:双核 Arm Cortex-A15 和双核 DSP、多媒体 AM5746 Sitara 处理器:双核 arm Cortex-A15 和双核 DSP,支持 ECC 的 DDR 和安全引导 AM5748 Sitara 处理器:双核 arm Cortex-A15 和双核 DSP,多媒体、支持 ECC 的 DDR 和安全引导 AM5749 Sitara 处理器:双核 Arm Cortex-A15 和双核 DSP、多媒体、支持 ECC 的 DDR、安全引导、深度学习

文档

Instructions for creating an SD Card with Linux

Instructions for creating an SD Card with Windows

Link to Release Notes for Processor SDK Linux

Link to the online Software Developers Guide which has the latest content

Link to the Linux Porting Guide for AM571x/AM570x Speed Grades

Software Manifest of Components Inside the SDK

发布信息

Thank you for your interest in the AM57x Software Development Kit (SDK). If you would like to install the full SDK on a Linux Host computer for development, you'll need the AM57x Linux SDK Essentials below. If you would like to evaluate the SDK by running it on one of the below platforms and you prefer not to install the full SDK at this time, please see the AM57x Linux SDK SD Card Creation section below.

More Information If you'd like more information on all of these choices, please refer to the Processor SDK Linux Getting Started Guide (GSG) below or the latest version here . For a complete overview of the SDK, please refer to the Processor SDK Linux Software Developer's Guide (SDG) below or the latest version here .