抬头显示

产品和参考设计

抬头显示

方框图

概述

An automotive head-up display (HUD) provides information to the driver at eye level. This allows the driver to continue looking at the road while getting speed and other information. The HUD is either projected on a section of the windshield or on a transparent surface between the driver and the windshield. More sophisticated HUDs are used to create the appearance of an overlay on the road for turn-by-turn navigation. The HUD information is typically provided by the cluster. We have the technology to power, connect and create the HUD display.

设计要求

Modern HUD designs require:

  • Digital light processors (DLP) to create the highest quality display.
  • High-efficiency power supplies for all HUD power requirements including LED display illumination.
  • Motor drivers for HUD positioning.
  • High-speed serial receivers for data interface enable higher bandwidth operation and reduce cabling cost.
  • Temperature sensors that monitor ambient temperature to ensure equipment runs at proper conditions.
  • Optical light sensors control dimming to improve display clarity in dynamic lighting environments.

下载 观看带字幕的视频 视频

方框图

查找适用于您系统的产品和参考设计

技术文档

查看所有 11
未找到结果。请清除搜索,并重试。
类型 标题 下载最新的英文版本 日期
功能安全信息 Making Cars Safer Through Technology Innovation (Rev. A) 2022年 7月 28日
更多文献资料 Achieving Low IQ Voltage Supervision in Automotive, Wide-Vin Applications 2022年 5月 11日
选择指南 Automotive Infotainment EE Buck Converter/Controller Selection Guide (Rev. B) 2021年 5月 21日
更多文献资料 Using Transimpedance Amplifiers for Ambient Light Sensing in Automotive Displays (Rev. A) 2019年 8月 23日
Technical articles Getting the most out of your power stage at the full temperature range – part 1 2019年 6月 7日
更多文献资料 设计互动无干扰的信息娱乐系统 下载英文版本 2019年 3月 15日
更多文献资料 DLP® 技术:增强现实抬头显示系统中的太阳能负载 下载英文版本 2018年 7月 23日
更多文献资料 DLP® Technology: Enabling the Next Generation of Automotive Head-Up Display Syst (Rev. A) 2017年 11月 15日
Technical articles You can be an electromechanical engineer 2017年 11月 10日
Technical articles Engineering magic: Touch through thick glass with LEDs and LCD 2016年 8月 18日
Technical articles Keep a watchful eye on your house with the Blink smart home monitoring system 2016年 1月 6日

支持与培训

视频