• Menu
  • Product
  • Email
  • PDF
  • Order now
  • GaN Applications

    • SLUAAM2 August   2022 LM5113-Q1 , LMG1020 , LMG1025-Q1 , LMG1205 , LMG1210 , UCC27611

       

  • CONTENTS
  • SEARCH
  • GaN Applications
  1.   1
  2. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
APPLICATION BRIEF

GaN Applications

Gate drivers are applicable in a wide variety of industry applications. The introduction of GaN has allowed many of these applications to experience improved performance by enabling designers to create more efficient and compact designs that can be driven at higher frequencies. This application brief provides some details of industry applications that have benefited from GaN and how they have improved.

LIDAR Application

Light detection and ranging (LIDAR) has many applications and can be used in automotive, robotics, drones, range finders, retinal imagers, surveying equipment, speed measurement devices, and much more.

LIDAR operates by using light in the form of a pulsed laser to detect objects and map their distances, which is why it is sometimes referred to as time of flight. There is a transmission system that sends out a short high-current light pulse. This pulse will bounce off of objects and eventually return to a receiver. The time between the signal leaving and returning can then be used to calculate the distance the pulse traveled. Transmitting signals faster will result in more accurate results since more data can be interpreted by the receiver. Gate drivers help send multiple pulses at very high speeds since they can operate at high frequencies.

GUID-20220729-SS0I-B7SL-WTVN-0VTNNJV8DKNG-low.pngFigure 1-1 LIDAR Transmission and Receiver Functionality

Low side drivers tend to be common for LIDAR applications. Two recommended gate drivers for LIDAR are the LMG1020 and LMG1025-Q1 GaN gate drivers. These two gate drivers are ideal for GaN applications since they are capable of high frequency applications, ns pulse widths, and have a short propagation delay. They are able to drive a FET to produce a <1.5-ns laser optical pulse in excess of 100 W, making them great for LIDAR applications. Figure 1-2 shows a block diagram of a general LIDAR application from the TIDA-01573 reference design. Some of the key components include a pulse shortening buffer for to create ns pulse widths, the GaN gate driver, the GaN FET, and the laser diode. The driver will pulse the FET on and off so that the laser diode can send multiple pulses to map objects and their distances.

GUID-20220729-SS0I-H6W1-5VR1-7MLDPCXHWVCQ-low.pngFigure 1-2 TIDA-01573 Reference Design Block Diagram

The schematic for TIDA-01573 reference design is shown in Figure 1-3. The LDO takes a VDD voltage input from 5.5 V – 15 V and provides a 5 V output, which is then used as a voltage supply to power up the driver. One key piece from this schematic is the addition of an input buffer which is needed to create ns pulse widths. The output of the driver is then connected to the gate of a GaN FET. Lastly, the load of the laser diode is represented by R5-R8.

GUID-20220729-SS0I-L6FQ-ZXFX-2CZJ3BKSLRFR-low.pngFigure 1-3 TIDA-01573 LIDAR Schematic
GUID-20220729-SS0I-L4HH-BGMS-4J2FPJHNKTZ9-low.pngFigure 1-4 Input Buffer for Nano Second Pulses

Creation of Nanosecond Pulse Widths

This section explains how the input buffer from the schematic works. Figure 1-4 shows a close up view of the input buffer. In this case, the INM pin of the driver in Figure 1-3 is tied to ground to serve as an enable, therefore the output of the driver will be high whenever the INP signal goes high. This method requires an RC filter and an AND gate. The PWM signal is connected directly to AND+. Then there is a RC filter placed between the PWM signal and AND- which delays the signal that goes into the AND- pin. When the PWM input signal is high, the AND gate’s positive input will also be high, whereas the signal at the AND gate’s negative input will gradually increase as it will be affected by the RC filter connected between the PWM signal and the AND gate’s input.

A timing diagram of the buffer is shown in Figure 1-5. When both inputs of the AND gate are higher than the gate’s threshold voltage, the IN+ (INP) input of the driver will go high causing the output of the driver to go high. When the PWM signal goes low, the AND+ signal will provide a quicker turn off since there is nothing to slow it down, therefore the output will go low when the AND+ signal drops below the threshold voltage. The period in between when both input signals (AND+ & AND-) are above the threshold voltage will dictate the time that the signal is on which can be used to generate a 1-2 ns pulse at the input, and therefore cause the same response at the output.

GUID-20220729-SS0I-KT6V-VHJQ-ZJFS3GQDCBXT-low.pngFigure 1-5 Input Buffer Timing Diagram

An alternate way to create a 1ns pulse is by using two input signals for the driver. For this to work, one of the signals will have to be delayed, in the case of Figure 1-6 it is the IN- signal. For reference, the output will follow the IN+ signal when IN- is low. The timing diagram in Figure 1-6 shows that IN+ is the leading signal so it will go high first, which will cause the output to go high as well. After a short delay, the IN- signal will go high and since both driver inputs are high the output will go low. The delay between the two input signals going high, as shown by the red dotted lines in Figure 1-6, will be the time the output is high, therefore if the delay between the two signals going high is 1ns then the output will be high for 1ns. This could then be done repeatedly to generate multiple nanosecond pulses.

GUID-20220729-SS0I-D1LL-2WMV-7C647BB8LFQ2-low.pngFigure 1-6 Nano Second Pulse Timing Diagram with Delayed Signal

DC/DC Converters Application

Switching regulators are the most efficient way to convert one DC voltage to another DC voltage. DC/DC converter are used for many things such as for step-down (buck) regulators, step-up (boost) regulators, buck-boost regulators, and inverting regulators. Switching-mode power supply designers are always pursuing higher power density, which requires higher frequency and efficiency.

GaN in DC/DC Converter

Compared to Si FETs, GaN high electron mobility transistors (HEMTs) exhibit smaller gate charge, faster switching, and no reverse recovery loss making them more advantageous for switching-mode power supply designers.

An example of the use of GaN for a DC/DC converter can be seen in the TI Design: TIDA-01634. This reference design uses GaN power HEMTs and a latest generation driver, the LMG1210 GaN half-bridge driver, to realize a multi-MHz synchronous buck converter with high efficiency. This buck converter can realize 3 ns of minimum on-time and up to a 50 MHz operation frequency. This design also provides driver UVLO and overtemperature protection.

Applications of TIDA-01634

With high-efficiency switching and flexible dead-time adjustment, this design can significantly improve power density while achieving good efficiency as well as wide control bandwidth.

This design can be applied to many space-constrained and fast response required applications such as high-speed synchronous buck converters, 5G telecom power, 48-to-POL server power, industrial power supplies, Class D audio amplifiers, and envelope tracking.

GUID-20220729-SS0I-FR67-MMG8-FZ11FSC4MVDQ-low.pngFigure 1-7 Block Diagram of the Synchronous Buck Converter

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2022, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale