Texas Instruments DLP technology is a micro- electro-mechanical systems (MEMS) technology that modulates light using a digital micromirror device (DMD). DMDs vary in resolution and size and can contain over 8 million highly reflective, digitally switchable, micrometer-sized mirrors (micromirrors) organized in a two-dimensional array (Figure 1).
Each micromirror on a DMD can represent one or more pixels on the screen and is independently modulated to create stunning displays. DLP technology powers the displays of products worldwide, from digital cinema and home theater projectors to virtual reality devices, digital signage, automotive heads-up displays, and more. TI DLP chipsets can enable bright, high resolution, portable displays of every size.
Laser TV is a new class of display products that combines innovations in three key areas: DLP technology with a laser light source, internet connectivity, and smart application-based operating systems. Combining these three technologies allows users to display a plethora of multimedia content onto screens or virtually any surface with typical display sizes of over 100-inches diagonal.
Laser TVs can be configured with ultra short throw optical modules allowing the product to be placed inches away from a display surface while still displaying a stunning image (see Figure 2).
For consumers who travel frequently or live in small homes, laser TVs with embedded wireless
capabilities can stream all types of online content on a huge screen while remaining very portable. This new generation of TVs provides consumers with the flexibility to move their display anywhere, including outdoors. For example, imagine sharing the big game experience or your favorite streaming content on a garage door with your neighbors and friends (see Figure 2).
Laser TV products can also be embedded into furniture (see Figure 2) or inconspicuously blended with décor for consumers who do not want a TV mounted on the wall but still want a large display.
Using DLP technology, developers can not only create a standalone laser TV but they can integrate a laser TV display to almost any electronic device.
DLP technology offers several key advantages that make it a great fit for laser TV:
This provides a developer with the flexibility to design differentiating products across different brightness, size, resolution, and cost levels.
For more information, see the Introducing BrilliantColor™ Technology white paper.
Ifan application requires size optimization or ultra portability in controlled lighting environments, check out the DLP® Technology for Mobile Smart TV white paper.
A typical laser TV projection system is comprised of four main components:
Front end processor –consists of an application processor that provides customized functionality such as:
DLP optical modules of various designs, sizes, capabilities,and performance are available from a number of optical module manufacturers (OMMs) who are part of the DLP ecosystem. The availability of existing optical modules accelerates the product development cycle of an end equipment producer because an appropriate DLP optical module can be utilized or adapted for use in the end product without requiring in-house expertise or resources. DLP design houses and some OMMs also have the ability to design and build a custom optical module for applications that require it.
Brightness is a measure of how much light is perceived by the human eye in a given scene and it is an important consideration when selecting a DLP chipset. This is a function of the amount of light (number of photons) and its spread across the color spectrum (photon energy), as well as the varying sensitivity of the human eye across the visible spectrum. The SI unit of brightness is the lumen (see ) can help determine the requirements based on screen size and ambient light conditions.
The level of detail available in an image is determined by the number of pixels which make up the displayed image. In a DLP system, this is a function of the number of mirrors on the DMD which can represent one or more pixels on the display. Resolution is the number of pixels that can be displayed. The level of detail displayed is not only dependent on the projector system but it is also dependent on the resolution of the source content. If the source content does not match the resolution of the projector system, then the source content is mapped by the controller to make maximum usage of the resolution displayed.
The quality of a viewed image is greatly determined by the distinction between the brightest and the darkest areas of the viewed image. This is quantified by the contrast ratio. While the contrast ratio specification of a DLP system is based on system performance, the viewing experience can also be greatly impacted by ambient light. The more ambient light on the screen, the lower the viewable contrast of the image. Together, system contrast and ambient light determine the true viewable contrast of the image. Special attention must be given to the optical design, and quality of optics used in the optical module to maximize contrast.
In many projection applications, the placement of the projector with respect to the viewing screen is important. The throw ratio of the projector determines how far away the projector must be placed in order to achieve a certain screen size (see Figure 7). The width of the projected image (W) with respect to the distance from the lens to the center of the screen (D) is the throw ratio (T), which is shown in Figure 7. Laser TV applications typically have ultra-short throw optical modules that allow for throw ratios of less than 0.4.
A major advantage of laser TVs is the ability to transport the compact device to any location versus a heavy traditional display system.
Depending on the design, the size and form factor of a laser TV device can be reduced. Higher brightness and resolution can result in additional thermal management in the form of heat sinks and fans which add to the overall size. When the right design considerations and trade-offs are made, a laser TV can be put into a form factor that can satisfy most every use case.
With a laser TV, any surface, whether it is a wall, portable screen, or a permanent wall-mounted screen, can enable a viewing experience. Projection screens are usually made of white fabric or even as screen paint that is applied to a wall. Adding a screen can limit how ambient light affects the projected image, having a significant impact on image quality. Projection screens can even be custom made to fit a specific design.
The DLP chipsets in Table 1 are well suited for laser TV applications.
DMD | Controller | System brightness (max) (lm) | Array diagonal (in) | Input frame rate (max) (Hz) |
---|---|---|---|---|
4K UHD resolution | ||||
DLP472TP | DLPC8445 | 2,000 | 0.47 | 60 |
DLP472TE | DLPC7540 | 6,000 | 0.47 | 60 |
DLP780TE | DLPC4420 | 7,000 | 0.78 | 60 |
DLP650TE | DLPC7540 | 8,000 | 0.65 | 60 |
DLP781TE | DLPC4420 | 13,000 | 0.78 | 60 |
1080p resolution | ||||
DLP230NPSE | DLPC3436 | 220 | 0.23 | 60 |
DLP230NP | DLPC3436 | 450 | 0.23 | 60 |
DLP3310 | DLPC3437 | 800 | 0.33 | 60 |
DLP4710 | DLPC3439 | 1,800 | 0.47 | 120 |
DLP650NE | DLPC4430 | 5,000 | 0.65 | 120 |
DLP472NE | DLPC7530 | 6,000 | 0.47 | 240 |
DLP780NE | DLPC4430 | 7,000 | 0.78 | 120 |
DLP651NE | DLPC7540 | 8,000 | 0.65 | 240 |
DLP781NE | DLPC4430 | 13,000 | 0.78 | 120 |
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2024, Texas Instruments Incorporated