DLPC105B September   2018  – June 2024 DLP470NE , DLP470TE , DLP471NE , DLP471TE , DLP472NE , DLP472TE , DLP472TP , DLP473NE , DLP650NE , DLP650TE , DLP651NE , DLP660TE , DLP780NE , DLP780TE , DLP781NE , DLP781TE

 

  1.   1
  2.   What is DLP technology?
  3.   What is laser TV?
  4.   Laser TV features
  5.   DLP technology for laser TV
  6.   System and electronics
  7.   Design considerations
    1.     Brightness
    2.     Resolution
    3.     Contrast
    4.     Throw Ratio
    5.     Size and form factor
  8.   Display surfaces
  9.   DLP chipsets for laser TV
  10.   Additional resources

Throw Ratio

In many projection applications, the placement of the projector with respect to the viewing screen is important. The throw ratio of the projector determines how far away the projector must be placed in order to achieve a certain screen size (see Figure 7). The width of the projected image (W) with respect to the distance from the lens to the center of the screen (D) is the throw ratio (T), which is shown in Figure 7. Laser TV applications typically have ultra-short throw optical modules that allow for throw ratios of less than 0.4.

 Brightness table. Figure 6 Brightness table.
 Throw ratio. Figure 7 Throw ratio.