ZHCSOK6B February 2017 – July 2024 CC3120
PRODUCTION DATA
The 3-wire UART topology requires only the following lines (see Figure 7-19):
Figure 7-19 3-Wire UART TopologyUsing this topology requires meeting one of the following conditions:
Because there is no full flow control, the host cannot stop the SimpleLink device to send its data; thus, the following parameters must be carefully considered: