SWRA732 December   2021 CC1352P , CC1352R , CC1354P10 , CC1354R10 , CC2642R , CC2652R , CC2652R7 , CC2652RSIP

 

  1.   Abstract
  2.   Trademarks
  3. 1 Introduction
  4. 2 Reference Examples
  5. 3 Software Block Diagram
  6. 4 Network Topology and Features
  7. 5 Security
  8. 6 Performance and Test Data
    1. 6.1 Hardware Setup
    2. 6.2 Software Setup
  9. 7 Power Consumption of the Low Power Node (LPN)
  10. 8 Out-of-Box Experience
  11. 9 Tools
  12. 10Known Limitations
  13. 11References

Network Topology and Features

TI’s Bluetooth mesh solution supports all node features defined by the specification, including:

Node Features Supported
Relay Yes
Proxy Yes
Friend Yes
Low Power Yes

As part of the specification [3], nodes can be configured to support multiple node features at one time. For example, a node can be configured to support Proxy features and Relay Features. However, a node configured as a Low Power Node may not be configured for any additional role.

TI’s Bluetooth mesh solution also supports the following Bluetooth SIG [1] defined models. At this time, the below models are supported by TI but not qualified by the Bluetooth SIG (with the exception of Foundation models) [1]. In addition to the below list, TI supports the creation of custom Vendor models as well.

Table 4-1 TI Bluetooth Mesh Model Support Summary
Model Group Mesh Models Supported
Foundation Foundation Models (configuration & health server/client) Yes
Vendor Custom Vendor Model Yes
Generic Generic OnOff Server Yes
Generic OnOff Client Yes
Generic Level Server Yes
Generic Level Client Yes
Generic Default Transition Time Server Yes
Generic Default Transition Time Client Yes
Generic Power OnOff Server Yes
Generic Power OnOff Setup Server Yes
Generic Power OnOff Client Yes
Generic Power Level Server No
Generic Power Level Setup Server No
Generic Power Level Client No
Generic Battery Server Yes
Generic Battery Client Yes
Generic Location Server No
Generic Location Setup Server No
Generic Location Client No
Generic Admin Property Server No
Generic Manufacturer Property Server No
Generic User Property Server No
Generic Client Property Server No
Generic Property Client No
Sensor Sensor Server Partial
Sensor Client Partial
Sensor Setup Server No
Time and Scenes All No
Lighting All No

Our solution supports provisioning over both GATT (PB-GATT) and Advertisement (PB-ADV) Bearer’s, as defined in the Bluetooth Mesh Profile Specification [3].