SSZT496 September 2019 TMS320F280041 , TMS320F280041C , TMS320F280045 , TMS320F280049C , TMS320F28075 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377S , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379S
C2000™ microcontrollers (MCUs) have been used to control motors in a huge variety of applications for over 25 years. These motors are primarily three-phase synchronous or asynchronous, and typically controlled using a technique called field-oriented control (FOC) to minimize power usage by providing efficient torque production. They are used in products ranging from sub-100-W medical tools up to hundreds of kilowatts industrial machinery. Some applications require only torque control, others a stable velocity, and still others very precise position control. Such disparate requirements require varied solutions, which TI has provided over the years through its digital motor control library, controlSUITE™ library and most recently MotorWare™ library.
Starting today, we are unifying our latest motor-control developments with device-level software drivers into a single product: the C2000Ware MotorControl software development kit (SDK).
This SDK supports the latest generation-compatible TMS320F28379D, TMS320F28076 and TMS320F280049C series in the C2000 platform, as well as all new series going forward. Components of the SDK include:
The InstaSPIN-FOC solution (fig 1) was released in 2013 and is enabled by an on-chip read-only memory (ROM) library on the F2806x, F2805x and F2802x series through the MotorWare software package. The library has been rewritten into floating point – removing the fixed-point scaling burden and taking advantage of on-chip accelerators – and updated in on-chip ROM for the F28004x series. Library function calls and step-by-step lab projects will look familiar to InstaSPIN-FOC users. TI has also released a new BoosterPack™ plug in module to work specifically for InstaSPIN-FOC solution with our C2000 Piccolo™ MCU F280049C LaunchPad™ development kit.
Figure 1 InstaSPIN-FOC FeaturesDesignDRIVE (fig 2) was released in - and has been routinely updated through - controlSUITE software suite. With its inclusion in the MotorControl SDK, we are now able to add support for C2000Ware. This gives a more complete and user-friendly software experience and enables easier porting of DesignDRIVE onto other C2000 MCU series.
Figure 2 Designdrive ComponentsThis first release of the MotorControl SDK includes the support shown in Figure 3.
Figure 3 MotorControl SDKTI will update the MotorControl SDK quarterly or biannually, and in future releases plans to support: