SPVA065 June 2026 TIC12400-Q1
When an INx channel is selected by the internal MUX, the internal voltage divider and ADC front-end circuitry are suddenly connected to the INx pin. During the sampling window (Tadc or Tcomp), a leakage current up to the ILKG bound is injected into the total capacitance present at the INx node. This total capacitance (CIN) includes the parasitic capacitance of the PCB trace and the TIC12400-Q1 pin, as well as any external filter capacitor intentionally added to the node. At the end of the sampling window, the MUX disconnects the internal front-end, and the stored charge discharges through the external source impedance (REXT) back toward the steady-state voltage defined by the external network. Figure 4 shows the resulting narrow voltage spikes measured at the INx pin across multiple polling cycles.
Figure 4-1 Repeating INx Voltage Spikes Across Polling Cycles — ADC ModeBecause the leakage current injection occurs consistently at each polling event and the REXT × CIN discharge time constant can be long relative to the polling interval, the INx node may not fully recover to its steady-state voltage before the next sampling event. This leads to a quasi-static DC offset superimposed on the true input voltage.