SPRZ487G May   2022  – October 2025 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP

 

  1.   1
  2. 1Usage Notes and Advisories Matrices
    1. 1.1 Devices Supported
  3. 2Silicon Usage Notes and Advisories
    1. 2.1 Silicon Usage Notes
      1.      i2351
      2.      i2330
      3.      i2372
      4.      i2424
    2. 2.2 Silicon Advisories
      1.      i2049
      2.      i2062
      3.      i2097
      4.      i2103
      5.      i2134
      6.      i2189
      7.      i2196
      8.      i2232
      9.      i2244
      10.      i2310
      11.      i2311
      12.      i2327
      13.      i2328
      14.      i2279
      15.      i2307
      16.      i2320
      17.      i2329
      18.      i2208
      19.      i2249
      20.      i2278
      21.      i2312
      22.      i2366
      23.      i2371
      24.      i2253
      25.      i2283
      26.      i2383
      27.      i2401
      28.      i2407
      29.      i2409
      30.      i2410
      31.      i2413
      32.      i2414
      33.      i2415
      34.      i2416
      35.      i2417
      36.      i2418
      37.      i2419
      38.      i2420
      39.      i2421
      40.      i2422
      41.      i2423
      42.      i2435
      43.      i2431
      44.      i2457
      45.      i2160
      46.      i2436
      47.      i2482
      48.      i2464
  4.   Trademarks
  5.   Revision History

i2160

DDR: Valid VRef Range Must be Defined During LPDDR4 Command Bus Training

Details:

The DDR PHY updates VREF(ca) for the command/address bus during LPDDR4 Command Bus Training (CBT). If VREF(ca) search range is set to invalid values such as no working settings can be found during CBT, the training process could fail or hang.

Workaround(s):

Set the following fields to known valid working values before enabling CBT.

For frequency set 0: PI_CALVL_VREF_INITIAL_START_POINT_F0 and PI_CALVL_VREF_INITIAL_STOP_POINT_F0

For frequency set 1: PI_CALVL_VREF_INITIAL_START_POINT_F1 and PI_CALVL_VREF_INITIAL_STOP_POINT_F1

For frequency set 2: PI_CALVL_VREF_INITIAL_START_POINT_F2 and PI_CALVL_VREF_INITIAL_STOP_POINT_F2

Recommendation is to use the nominal VRef value (based on the device programming of drive strength on the processor and termination in the memory) +/- 4%. Please use the online DDR Register Configuration Tool at http://dev.ti.com/sysconfig to program these registers and check the Revision History to ensure this workaround has been addressed in the version of the tool being used.