SPRZ487G May 2022 – October 2025 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP
OSPI: Controller PHY Tuning Algorithm
The OSPI controller uses a DQS signal to sample data when the PHY Module is enabled. However, there is an issue in the module which requires that this sample must occur within a window defined by the internal clock. Read operations are subject to external delays, which change with temperature. To ensure valid reads at any temperature, a special tuning algorithm must be implemented which selects the most robust TX, RX, and Read Delay values.
The workaround for this bug is described in detail in SPRACT2. To sample data under some PVT conditions, users are required to increment the Read Delay field to shift the internal clock sampling window. This allows sampling of the data anywhere within the data eye. However, this has these side effects: