SPRZ455F December 2020 – February 2025 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1
UDMAP: Spurious ECC errors due to MAIN/MCU NAVSS rofifo_wr_byten issue
Packet Starvation can cause a spurious ECC error. If a packet is received and there is no current descriptor to send the packet, the UDMAP sends out a single byte memory read to a predefined memory address to allow for update scoreboards. The received read data will update the buffer memory for the channel without updating the ECC signature stored in the channel FIFO memory. When the channel FIFO does the read to reclaim the buffer, an ECC error is generated by the hardware.
If all the flows set rx_error_handling mode to 1 in the RX Flow Configuration Register, this will disable the dummy read as the logic now waits for a descriptor instead of generating an error. If it is required that error handling mode is 0 and packet drops are reported, then the software must clear the ECC error after receiving a dropped packet count increment.