SPRZ455D december 2020 – june 2023 DRA829J , DRA829J-Q1 , DRA829V , TDA4VM , TDA4VM-Q1
ADVANCE INFORMATION
USB: Endpoint OUT Data Queue is Locked Up Due to a Data
Packet for an Endpoint that Does Not Have Associated TRB
The USB device controller stores the endpoint OUT data received on the USB bus into a queue data structure. It transfers the data from the queue to system memory if a Transfer Request Block (TRB) is available for the endpoint that owns the data. However, if a TRB is not available for this endpoint, the data stays in the queue and blocks the subsequent data in the queue from being transferred to system memory. This occurs even if the endpoints owning the subsequent data have TRBs available.
One known use case which could be affected by this issue is a composite device that combines ACM class with another class such as MSC. ACM class drivers are known to operate without TRBs for long durations. If the other class receives data after the ACM class, it could potentially be stuck in the queue until the ACM class driver provides its TRB. This issue could be observed in general with classes that do not provide a TRB in advance or may not provide a TRB for long durations after data is received.
An IRQ[6] interrupt is generated by the Controller when data is received into the queue for an endpoint that does not have a TRB. The corresponding interrupt status bit for this register is called the TRBERR in EP_STS register. Software can potentially use this interrupt to provide a TRB for the blocking endpoint. If the data is not needed immediately, the software must configure the TRB such that the data is transferred from the queue to a temporary buffer in the system memory. The data in the system memory can be consumed at a later time.