SPRZ455D december 2020 – june 2023 DRA829J , DRA829J-Q1 , DRA829V , TDA4VM , TDA4VM-Q1
ADVANCE INFORMATION
C71x: Register Corruption When MMA HWARCV is in Parallel With
Load or Store With uTLB Miss
The C71x has the possibility of data corruption for certain circumstances on an HWARCV instruction. The symptom is that every 8th byte of the 64Bytes of data from the HWARCV data is corrupted with an arbitrary result (every 8th starting from the least significant byte of the vector). The value seen in the corrupting bytes is likely all zeros unless floating point instructions were executed previously on the .S2 unit.The condition under which this can occur has to do with three cases of resolving whether certain instructions that are in parallel with the HWARCV instruction must take extra time to determine whether the execution of that instruction will result in an exception, AND in the execute packet after this HWARCV instruction there is no instruction on the .S2 unit which will write a result into a 64 byte register.
When adding the compiler switch --silicon_errata_i2117 to the command line of the C71x compiler, the compiler automatically ensures that there is an instruction on the .S2 unit that writes to a 64 byte vector register following all HWARCV .S2 instructions. This action ensures that one of the required conditions for encountering this issue is not met. If there is no useful work to be performed, the compiler inserts a dummy instruction which writes to an unused register, and is effectively a NOP instruction.