SPNU118Y September 1995 – February 2020
Symbol mapping allows a symbol reference to be resolved by a symbol with a different name. Symbol mapping allows functions to be overridden with alternate definitions. This feature can be used to patch in alternate implementations, which provide patches (bug fixes) or alternate functionality. The syntax for the --symbol_map option is:
--symbol_map=refname=defname
For example, the following code makes the linker resolve any references to foo by the definition foo_patch:
--symbol_map='foo=foo_patch'
The --symbol_map option is now supported even if --opt_level=4 was used when compiling.