SPNU118Y September 1995 – February 2020
The --generate_dead_funcs_list option creates a list of functions that are never referenced (dead) and writes the list to the specified file. If no filename is specified, the default filename dead_funcs.xml is used. The syntax for the option is:
--generate_dead_funcs_list=filename
Refer to the ARM Optimizing C/C++ Compiler User's Guide for details on the --generate_dead_funcs_list option and the corresponding --use_dead_funcs_list option.