SPNU118Y September 1995 – February 2020
These directives set up specialized types for later use in expressions allowing you to use symbolic names to refer to compile-time constants. The types created are analogous to the enum type of the C language. This allows enumerated types to be shared between C and assembly code. See Section 13.
See Section 13.2.10 for an example of using .enum.