SPNU118Y September 1995 – February 2020
The following built-in substitution symbol functions enable you to make decisions on the basis of the string value of substitution symbols. These functions always return a value, and they can be used in expressions. Built-in substitution symbol functions are especially useful in conditional assembly expressions. Parameters of these functions are substitution symbols or character-string constants.
In the function definitions shown in Table 6-1, a and b are parameters that represent substitution symbols or character-string constants. The term string refers to the string value of the parameter. The symbol ch represents a character constant.
| Function | Return Value |
|---|---|
| $$symlen(a) | Length of string a |
| $$symcmp(a,b) | < 0 if a < b; 0 if a = b; > 0 if a > b |
| $$firstch(a,ch) | Index of the first occurrence of character constant ch in string a |
| $$lastch(a,ch) | Index of the last occurrence of character constant ch in string a |
| $$isdefed(a) | 1 if string a is defined in the symbol table |
| 0 if string a is not defined in the symbol table | |
| $$ismember(a,b) | Top member of list b is assigned to string a |
| 0 if b is a null string | |
| $$iscons(a) | 1 if string a is a binary constant |
| 2 if string a is an octal constant | |
| 3 if string a is a hexadecimal constant | |
| 4 if string a is a character constant | |
| 5 if string a is a decimal constant | |
| $$isname(a) | 1 if string a is a valid symbol name |
| 0 if string a is not a valid symbol name | |
| $$isreg(a)(1) | 1 if string a is a valid predefined register name |
| 0 if string a is not a valid predefined register name |
Example 5 shows built-in substitution symbol functions.