SNVAA30 December 2021 LM5170-Q1
Battery equalizer has two modes to support stable power for both 12-V and 24-V loads.
Constant voltage mode
Figure 1-2 shows constant voltage operation of battery equalizer. When 12-V loads are low-powered, namely Iload ≪ Imax, the 24-V load becomes the main load of the two batteries. The battery equalizer keeps Batt_B voltage to be right at 50% of the total voltage of the two series batteries, such that the two battery capacities get well-balanced.
Figure 1-2 Constant Voltage Mode of Battery EqualizerConstant current mode
Figure 1-3 shows constant current operation of battery equalizer. When 12 V loads consume high power, Batt_B is consumed faster than Batt_T. The battery equalizer will produce 12-V load current to prevent Batt_B from being discharged, therefore the two batteries remains the voltage balance. Obviously, the battery equalizer should provide Iout = Imax.