SNOU143 February 2017
The EVMs are connected using a standard wire jumper; Figure 6 shows the connections between the two EVMs. By default, the TMS570 LaunchPad is powered by the USB port on the host computer and the EM1402EVM is powered by a 3.3-V regulator on the TMS570 LaunchPad board.
| Connection Name | EM1402EVM | TMS570 LaunchPad | |||
|---|---|---|---|---|---|
| TX | J3 pin 5 | J1 pin 3 (SCI1_RX) | |||
| RX | J3 pin 4 | J1 pin 4 (SCI1_TX) | |||
| nWAKE | J3 pin 6 | J2 pin 3 (GIOA0) | |||
| nFAULT | J3 pin 2 | J2 pin 4 (GIOA1) | |||
| VIO | J3 pin 3 | J1 pin 1 (+3V3) | |||
| GND | J3 pin 1 | J2 pin 1 (DGND) | |||