SNIU039 December   2019

 

  1.   HDC2022EVM User's Guide
    1.     Trademarks
    2. 1 Quick Start
    3. 2 EVM GUI
      1. 2.1 Software Setup
        1. 2.1.1 Live Software on dev.ti.com
        2. 2.1.2 Offline Software
          1. 2.1.2.1 Download GUI from dev.ti.com
    4. 3 GUI Operation
      1. 3.1 Home Tab
      2. 3.2 Data Capture Tab
      3. 3.3 EVM Settings Tab
      4. 3.4 Device Configuration
      5. 3.5 Registers Tab
      6. 3.6 Collateral Tab
    5. 4 EVM Hardware
      1. 4.1 Input/Output Connector Description
        1. 4.1.1 J1 & J2 – 5x1 Headers
        2. 4.1.2 USB Type A Connector
      2. 4.2 EVM Operating Conditions
      3. 4.3 Device Address Configuration
      4. 4.4 Reducing the Sensor's Thermal Mass
    6. 5 Updating Firmware on HDC2022EVM
    7. 6 Board Layout
    8. 7 Schematic
    9. 8 HDC2022EVM Bill of Materials

Updating Firmware on HDC2022EVM

By default the HDC2022EVM will come programmed with the correct firmware for operation, the instructions in this section provide guidance on how to reflash the firmware in the event an upgrade is required, or if the board firmware has become corrupted because of misuse.

The primary method for flashing the HDC2022EVM is Spy-Bi-Wire. In order to reflash the firmware you will need the following:

To update the firmware on the HDC2022EVM complete the procedure below:

  1. Plug in the HDC2022EVM to the PC via USB Connector to provide power to the EVM.
  2. Connect another USB cable to the MSP-EXP430F5529LP
  3. Remove the SBW RST and SBW TST Jumpers on the MSP-EXP430F5529LP board
  4. Create a wiring harness by connecting jumpers to SBW RST, SBW TST, and GND on the MSP-EXP430F5529LP.
  5. Insert the male end of the jumpers through the SWBTCK, SBWTDIO, and GND through holes on the HDC2022EVM. These are shown in Figure 16. Make these connections as follows:
    • SBW RST ↔ SBWTDIO
    • SBW TST ↔ SBWTCK
    • GND ↔ GND
  6. HDC2022EVM_Front_SBWTCK_DIO.pngFigure 16. HDC2022EVM Spy-Bi-Wire programming connections
  7. Open UniFlash.
  8. Select MSP430F5528 as the target, select your connection and click Start
  9. SNIU039_UniFlash.pngFigure 17. UniFlash Launch Screen, MSP430F5528 device selected.
  10. Browse to the firmware file named USB2ANY-F5528-24MHZ.txt and select Load Image.
Upon successful programming, the firmware image will be loaded and the HDC2022EVM will automatically restart. The HDC2022EVM firmware upgrade is then complete.