SNAU218A November   2018  – August 2022

 

  1.   LMX2615EVM-CVAL Wideband 15-GHz Synthesizer
  2.   Trademarks
  3. Evaluation Board Setup and Description
  4. Setting Up the Software
  5. Bringing LMX2615 to a Lock State
  6. Current Loop Filter Configuration
  7. Typical Phase Noise
  8. Schematic
  9. Bill of Materials
  10. PCB Specifications
  11. Proper Jumper and Switch Positions
    1. 9.1 Reference Pro Board
  12. 10Revision History

Bringing LMX2615 to a Lock State

Load the default mode as shown in Figure 3-1 The PLL GUI tab gives useful feedback to the user that is helpful in getting the best performance out of the device

  • Items highlighted in orange or red indicate that something may be sub-optimal. To view the comment, simply mouse over the colored item and a tooltip will appear. In this case, the feedback suggests that CAL_CLK_DIV and VCO_SEL can be adjusted to improve the VCO calibration time, SEG1_EN could be disabled for better spurs and lower current, and that FCAL_EN should be toggled to calibrate the VCO.
  • Mouse over any item and it will display the field value in the lower left corner including the field name, register location, and description.
  • On the bottom is the status bar, which indicates when registers are written to and the status of the USB2ANY/Reference Pro board. In this case, it is indicating that there is no board connected.
GUID-6BF4C5BA-D9F4-4232-912C-5D02ED4D6C13-low.gifFigure 3-1 TICS Pro GUI LMX2615 Default Configuration

The GUI gives the user feedback to help them understand how to program and get the best performance out of this device.