SLVUDU7 April 2026 LMG708B0
TI recommends using one or more of the inner PCB layers as a solid ground plane. In particular, a full ground plane on the layer directly underneath the power-stage components is essential. Connect the exposed pads at the base of the LMG708B0 as well as the return terminals of the input and output capacitors to this ground plane. Keep PGND and AGND separate by using a dedicated island for AGND. The PGND nets contain high-frequency noise related to the high-di/dt switching currents. The power traces for VIN, PGND, and SW can be restricted to one side of the ground plane.