SLVUDC3 September 2025
To use the EVM with the TI-SCB Controller, connect the EVM as shown in Figure 3-1, or connect the EVM using one of the ways described in Section 2. The TMAG5134 output triggers when a magnet is near the sensor. When the magnetic field at the sensor crosses the threshold of the device, the output turns the LED on. The user can also check the output through the connector on the board.
Figure 3-1 EVM With Magnet