SLVUDB6A August 2025 – May 2026
The following section is a complete summary of the various headers and jumper connections on the TXE81XXEVM.
Figure 2-5 describes LED enable jumpers. If the header is left un-populated, the LED's for the specific port are disabled.
| Designator | Port # |
|---|---|
| J19 | Port 0 - LED Enable |
| J21 | Port 1- LED Enable |
| J23 | Port 2- LED Enable |
| J20 | Port 3- LED Enable |
| J22 | Port 4- LED Enable |
| J24 | Port 5- LED Enable |
Header J18 is used for programming the on-board USB2ANY circuit. For more details, see Figure 2-6.