SLVUCD3A November   2021  – August 2022 DRV8328

 

  1.   Abstract
  2. 1Introduction
  3. 2Quick Start Guide
  4. 3Hardware and Software Overview
    1. 3.1 Hardware Connections Overview – DRV8328AEVM + LAUNCHXL-F280049C
    2. 3.2 Connection Details
    3. 3.3 LED Lights
    4. 3.4 DRV8328AEVM Configurability and Switch Functions
      1. 3.4.1 DRV8328A/B Compatibility
      2. 3.4.2 DRV8328C/D Compatibility
    5. 3.5 Interfacing DRV8328AEVM and LAUNCHXL-F280049C LaunchPad
  5. 4Hardware Setup
  6. 5Firmware and GUI Application
    1. 5.1 Connecting to the DRV8328xEVM GUI
    2. 5.2 DRV8328AEVM GUI Quick Start Guide
    3. 5.3 Using the DRV8328AEVM-GUI
  7. 6Schematics
    1. 6.1  DRV8328A/B/C/D
    2. 6.2  DRV8328C/D variant select
    3. 6.3  Status LEDs
    4. 6.4  LaunchPad Connectors and Connections
    5. 6.5  External 3.3V LDO
    6. 6.6  Power Stage and MOSFETs
    7. 6.7  Main Supply Input
    8. 6.8  Hall Sensor and Hall Power Selection
    9. 6.9  Connectors, Selectors, and Analog Control Interface
    10. 6.10 Voltage Sense and Protection
  8.   Trademarks
  9. 7Revision History

Connecting to the DRV8328xEVM GUI

Follow the instructions in Section 5 and ensure the LAUNCHXL-F280049C is connected to the PC. Turned on the supply to power the DRV8328AEVM and LAUNCHXL-F280049C.

Access the GUI Composer Gallery and search for "DRV8328" as shown in Figure 5-1. Click on the version of the GUI depending of the DRV8328 variant configured on the EVM. If using the DRV8328AEVM out of the box, select the DRV8328A_DRV8328C_EVM_GUI tile on the left.

Figure 5-1 DRV8328AEVM GUI tiles in the Gallery for A, B, C, and D variants
Accept the readme that appears. The GUI will detect the LAUNCHXL-F280049C and automatically download the program into the MCU. Once complete, the “Hardware Connected” message appears at the bottom left hand corner as shown in Figure 5-2.

GUID-20220720-SS0I-HZR9-JH3N-8C6SLMVWFZFQ-low.pngFigure 5-2 Hardware Connected message in the bottom-left hand corner
As shown in Figure 5-3, the following defaults should appear when the GUI is connected:

  • Direction – Enabled

  • PWM Frequency (Hz) – 20000

  • MCU Dead Time (ns) – 0

  • Acceleration Delay (ms/1% duty cycle) – 21

GUID-20220720-SS0I-58CC-0VF1-FJKWDGJJ9SV4-low.pngFigure 5-3 DRV8328A_DRV8328C_EVM GUI loaded with default settings