SLVUC16 October   2020

 

  1.   Trademarks
  2. 1Introduction
    1. 1.1 Features
    2. 1.2 Applications
  3. 2Test Setup
    1. 2.1 The TLC6C5748EVM Kit
    2. 2.2 System/Equipment Requirements
    3. 2.3 Software Setup
    4. 2.4 Hardware Setup
    5. 2.5 Test Procedure
  4. 3Configuration of MCU Launchpad
  5. 4TLC6C5748EVM Board Layout
  6. 5TLC6C5748EVM Schematic
  7. 6TLC6C5748EVM Bill of Materials
  8. 7Revision History

Software Setup

Step 1: Download the CCS IDE and follow the installation instructions. Choose "SimpleLink MSP432 low power + performance MCUs components" when choosing support device if custom installation is selected, as shown in Figure 2-3.

GUID-20201021-CA0I-QKNC-R5LM-PTBZ3MVXD1DP-low.gif Figure 2-3 Select components when install CCS IDE

Step 2: Download and install the MSP432 SDK.

Step 3: Download the sample code from the TLC6C5748EVM tools folder and import the sample code according to the Importing a CCS Project steps.

Step 4: If the project can’t be imported, please try to install the latest version of ti-cgt.

Step 5: Power on the MSP-EXP432P401 Launchpad. The Launchpad should be connected to the PC as shown in Figure 2-5 using the Micro USB cable provided in the Launchpad kit. Debug the project and download the sample code to MSP-EXP432P401 Launchpad according to the Building and Running Your Project steps. Pressing the button shown in Figure 2-4 can also compile and debug the sample code. There will be no errors if all the previous steps are correct.

GUID-20201021-CA0I-V5CV-5WNJ-MBZDWNW8DD56-low.gifFigure 2-4 Compile and Debug Project in CCS IDE
GUID-20201021-CA0I-0RPH-5XHR-RZD1CTJ58SG8-low.gifFigure 2-5 Download the Sample Code to MCU

Step 6: Terminate the project and then power down the MCU.