SLVSMB0 June 2026
Standard commands are common commands from the Smart Battery Specification (SBS) industry-standard which defines smart battery interfacing. Standard commands use a command code pair to associate the registers associated with each command. Read and write commands should be addressed to the LSB of the command code.
Example: Read the RelativeStateOfCharge.
Figure 8-1 shows 0x3B 00 in the Data column of the Transaction Log sub-window. This value is 59 in decimal, corresponding to the RSOC%.
Figure 8-1 Standard Data Command Example