SLVK312 July 2026 DAC39RF10-SEP
The DAC was configured in JMODE3 and a baseline FFT was captured on the spectrum monitoring software (HSDCPRO) showing four unique tones (all four NCOs have been programmed) and typical analog performance. During the beam run, the DAC output was monitored by taking repeated captures with the HSDCPRO software. No degradation was observed during or after the beam run. This result shows that the DAC39RFx10-SEP is not susceptible to SEFI that would permanently corrupt the DAC performance. This also demonstrates that the internal calibration and trim vectors and configuration registers are not corrupted by radiation.
Figure 7-1 DAC39RFx10-SEP Baseline (Beam-Off) Performance and 4x NCOs Set for SEFI Testing
Figure 7-2 DAC39RFx10-SEP Performance Mid-Run