SLVK281 February   2026 SN54SC1G175-SEP

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Overview
  5. 2Single-Event Effects (SEE)
  6. 3Test Device and Test Board Information
  7. 4Irradiation Facility and Setup
  8. 5Results
    1. 5.1 Single-Event Latch-up (SEL) Results
    2. 5.2 Single-Event Transients (SET) Results
  9. 6Event Rate Calculations
  10. 7Summary
  11. 8References

Irradiation Facility and Setup

The heavy ion species used for the SEE studies on this product were provided and delivered by the Facility for Rare Isotope Beams (FRIB) at Michigan State University (FRIB Single Event Effects (FSEE) Facility’s linear accelerator.) The FSEE Facility has a dedicated beamline built on the FRIB linac infrastructure with a user experimental station at the end of the FSEE beamline. Ion beams are delivered with high uniformity over a 1-inch diameter exposure area using a thin vacuum window. For this study, ion flux of 1 × 105 ions / cm2-s was used to provide heavy ion fluence of 1 × 107 ions / cm2 using 129Xe ion at a linac energy of 25 MeV / µ. Ion beam uniformity for all tests was 96.42%.

Figure 4-1 shows one of the three SN54SC1G175-SEP test boards used for experiments at the MSU facility. The in-air gap between the device and the ion beam port window was maintained at 70mm for all runs.

 SN54SC1G175-SEP Evaluation Board at the MSU FacilityFigure 4-1 SN54SC1G175-SEP Evaluation Board at the MSU Facility
 SN54SC1G175-SEP Thermal Image for SELFigure 4-2 SN54SC1G175-SEP Thermal Image for SEL