SLVAFZ9 June 2026 TAC5212
When PurePath Console is launched, it queries the user on how many devices are connected to an AC-MB, as shown in Figure 4-3. In this dialog window, after selecting two TAC5212 devices and clicking on New, the main window shown in Figure 4-4 launches.
Figure 4-3 PurePath Console Input Number of Devices DialogPurePath Console configures only one device at a time. The devices are labeled by a device icon with a letter at the top of the screen, as shown in Figure 4-4. Clicking on device icon A programs the lower number I2C address, B programs the next I2C address, and so forth.
Figure 4-4 PurePath Console Main WindowThe Audio Serial Bus tab assigns each channel of a device to a slot. In Figure 4-5, the device A input channels 1-4 are assigned to slots 0-3, respectively. In Figure 4-6, the device B input channels 1-4 are assigned to slots 4-7. Note that the previous slots in the TDM bus are not shown, but an ellipsis at the beginning of the audio interface signal line plot in BCLK, FSYNC, and SDOUT signifies that other slots precede these slots.
Figure 4-5 PurePath Console Device A Channel to Slot Mapping
Figure 4-6 PurePath Console Device B Channel to Slot Mapping