SLVAF72 September   2021 TPS2661

 

  1.   Trademarks
  2. 1Overview of a HART Enabled Analog Input Module
  3. 2Protection Provided by TPS2661 to Analog Input Module
    1. 2.1 Overload Protection
    2. 2.2 Output Hot Short and Input Hot Plug
    3. 2.3 Miswiring on Input
    4. 2.4 Input Under Voltage Protection
  4. 3Protection Provided by TPS2661 to Analog Output Module (AOM)
    1. 3.1 Miswiring on Output
    2. 3.2 Output under voltage protection
  5. 4HART Tests Done on TPS2661x
  6. 5Challenges Using Discrete Solution Instead of TPS2661x

HART Tests Done on TPS2661x

To test the performance of TPS2661x on HART protocol, the approach was to check the impact TPS2661x have on the loop current and the HART communication bits that were being transmitted. To figure the possibility of bit error being introduced by TPS2661x, multiple strategies were adopted in putting together the data set for the test. The data set covered the possibility of bit swap and bit flip errors being introduced by TPS2661x leakage currents. A sample data set is shown in Figure 4-1 and Figure 4-2. The reference data point will be HART transmission between HART transceivers without the Loop current protector. This data would be compared with the data received after adding the TPS2661x current loop protector in the communication loop. Tests were performed with different dc loop current settings.

Data set included the following:

  • Single byte transmission
  • Transmission of byte sequence in ascending order from 00 to FF
  • Transmission of byte sequence in descending order from FF to 00

Results of the tests proved that, the low leakage current feature helped TPS2661x to provide the required protection without interfering with the analog dc loop current while allowing the HART communication. No bit flip or bit swap errors were also observed on HART communication with TPS2661x inserted in the communication loop. Figure 4-1 and Figure 4-2 show the HART communication through TPS2661x for a 0 and 1 transmission. Table 4-1 and Table 4-2 provide the HART data transmission results with TPS2661x device.

GUID-20210223-CA0I-KGWZ-BPLT-KGVK1DJQ5F6R-low.png Figure 4-1 1.2Khz HART Signal Through TPS2661x
GUID-20210223-CA0I-8SKG-KPLF-NTFNFP7GNLLB-low.png Figure 4-2 2.2Khz HART Signal Through TPS2661x
Table 4-1 Ascending Order HART Data
Write Byte Read Byte Error Byte Loop Current Write Byte Read Byte Error Byte Loop Current
Without TPS2661x With TPS2661x
0 0 No Error 4, 2.5, 7.5mA 0 0 No Error 4, 2.5, 7.5mA
1 1 No Error 4, 2.5, 7.5mA 1 1 No Error 4, 2.5, 7.5mA
2 2 No Error 4, 2.5, 7.5mA 2 2 No Error 4, 2.5, 7.5mA
3 3 No Error 4, 2.5, 7.5mA 3 3 No Error 4, 2.5, 7.5mA
4 4 No Error 4, 2.5, 7.5mA 4 4 No Error 4, 2.5, 7.5mA
5 5 No Error 4, 2.5, 7.5mA 5 5 No Error 4, 2.5, 7.5mA
6 6 No Error 4, 2.5, 7.5mA 6 6 No Error 4, 2.5, 7.5mA
7 7 No Error 4, 2.5, 7.5mA 7 7 No Error 4, 2.5, 7.5mA
8 8 No Error 4, 2.5, 7.5mA 8 8 No Error 4, 2.5, 7.5mA
9 9 No Error 4, 2.5, 7.5mA 9 9 No Error 4, 2.5, 7.5mA
A A No Error 4, 2.5, 7.5mA A A No Error 4, 2.5, 7.5mA
B B No Error 4, 2.5, 7.5mA B B No Error 4, 2.5, 7.5mA
Table 4-2 Descending Order HART Data
Write Byte Read Byte Error Byte Loop Current Write Byte Read Byte Error Byte Loop Current
Without TPS2661x With TPS2661x
FF FF No Error 4, 2.5, 7.5mA FF FF No Error 4, 2.5, 7.5mA
FE FE No Error 4, 2.5, 7.5mA FE FE No Error 4, 2.5, 7.5mA
FD FD No Error 4, 2.5, 7.5mA FD FD No Error 4, 2.5, 7.5mA
FC FC No Error 4, 2.5, 7.5mA FC FC No Error 4, 2.5, 7.5mA
FB FB No Error 4, 2.5, 7.5mA FB FB No Error 4, 2.5, 7.5mA
FA FA No Error 4, 2.5, 7.5mA FA FA No Error 4, 2.5, 7.5mA
F9 F9 No Error 4, 2.5, 7.5mA F9 F9 No Error 4, 2.5, 7.5mA
F8 F8 No Error 4, 2.5, 7.5mA F8 F8 No Error 4, 2.5, 7.5mA
F7 F7 No Error 4, 2.5, 7.5mA F7 F7 No Error 4, 2.5, 7.5mA
F6 F6 No Error 4, 2.5, 7.5mA F6 F6 No Error 4, 2.5, 7.5mA
F5 F5 No Error 4, 2.5, 7.5mA F5 F5 No Error 4, 2.5, 7.5mA
F4 F4 No Error 4, 2.5, 7.5mA F4 F4 No Error 4, 2.5, 7.5mA
F3 F3 No Error 4, 2.5, 7.5mA F3 F3 No Error 4, 2.5, 7.5mA