SLVAEX0 October 2020 TPS1H000-Q1 , TPS1H100-Q1 , TPS1H200A-Q1 , TPS1HA08-Q1 , TPS1HB16-Q1 , TPS1HB50-Q1 , TPS2HB16-Q1 , TPS2HB50-Q1 , TPS4H000-Q1 , TPS4H160-Q1
The devices that have a DELAY pin can be configured three ways: pulled directly to GND, pulled to GND through a capacitor, or pulled high through an external pull up. This allows for three modes for devices that have the DELAY pin: Holding, Latch-Off, and Auto-Retry as shown in Table 3-2.
The Latch-Off and Auto-Retry operate in similar modes as the LATCH behavior. Latch-Off mode will latch off after a configured delay time by grounding the DELAY pin through a capacitor. Auto-Retry will periodically attempt to restart normal operation after some time. The Holding mode is configured by grounding the DELAY pin and sets the device to hold the current limit until the device hits thermal shutdown.
Table 3-2 shows these modes, their behavior, and how to recover from them.
| Mode | Delay Configuration | Output Current Behavior | /Fault Recovery |
|---|---|---|---|
| Holding | Connect to GND directly | When hitting a current limit, the output current holds at the set current. The device enters into thermal shutdown mode when TJ > T(SD) | /Fault clears when IN turns low for a duration longer than t/FAULT OR when the current limit is removed when IN is high |
| Latch-Off | Connect to GND through a capacitor | When hitting a current
limit, the output current holds at the set current, but latches off
after a preset DELAY time (tdl1 + tdl2)
where The output stays
latched off regardless of whether the current limit is removed. The
output recovers when IN is toggling. |
/Fault clears when IN turns low for a duration longer than t/FAULT |
| Auto-Retry | External Pullup | When hitting a current limit, the output current holds at the set current, but periodically comes on for thic(on) and turns off for thic(off). | /Fault clears when IN turns low for a duration longer than t/FAULT OR when the current limit is removed for thic(on) |